This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507-Q1: SPI communication DRV3901-Q1

Part Number: MSPM0G3507-Q1
Other Parts Discussed in Thread: DRV3901-Q1

Tool/software:

Good day, colleagues,

My customer uses the MSPM0G3507-Q1 and DRV3901-Q1 and have the problem that a maximum framesize of 16 bits can be configured in CCS.
But the DRV3901 needs 24 bit frame size. They have an example code for the DRV3901 but only for the MSP430. The question is is this driver also available for the MSPM0G3507-Q1 or
would it be possible to realize the 24 bit framesize with the MSPM0G3507-Q1 or if there is an example code to generate a 24bit SPI communication interface between the 3507G and the DRV3901?

Thank you,

Daria