Part Number: AM2432
Tool/software:
Hi Expert,
customer want to use AM24 GPIO to drive a LED, so they want to know what the max current is we can output from GPIO? Thanks for support in advance.
BR,
Biao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Biao,
Thank you for the query.
You need to check
7.7.6 LVCMOS Electrical Characteristics
Please review the LED forward drop and LVCMOS Electrical Characteristics to verify the usability
You need to perform simulation in case the current draw is higher than the data sheet specs and this is not recommended. It is recommended to buffer the IO to drive higher LED current.
Regards,
Sreenivasa
Hi Sreenivasa,
In datasheet, only min value be defined. I can't see the max current. can you tell me what is the Max?

BR,
Biao
Hello Biao,
Thank you.
Not sure i understand the query.
We do not recommend loading the IO more than the current mentioned in the data sheet.
To understand the behavior with higher output load, it is recommended to perform simulations.
Regards,
Sreenivasa
Hello Biao,
Additional inputs for reference.
For background, this IOL/IOH spec is not meant to convey any information towards switching speed, actual current while driving capacitive load etc. Our IBIS model can be used to understand the transient characteristics of our IOs.
Rather, what the spec is trying to say (take the 1.8V spec as an example:)

We are able to drive a logic 1 and source "at least" (min) 3mA of current and still maintain a VOH higher than the min spec of VDD(1.8V)-0.45=1.35V. Similarly, to drive low ... we can sink at least 3 mA of current and still maintain a VOL lower than 0.45mv.
Considering 1.8V/3mA = 600 Ohm. That implies we can easily drive a PU/PD in the 2.2k to 10k range.
Regards,
Sreenivasa