This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM44L920: Implementing Safety Diagnostic Library to the project with bootloader

Part Number: RM44L920
Other Parts Discussed in Thread: HALCOGEN

Tool/software:

Hi,

I’m trying to integrate the Safety Diagnostic Library (SDL) into an existing project that already has a bootloader. The bootloader is based on TI's uart bootloader example. I’d appreciate some guidance on best practices for implementing SDL in this setup.

  1. Is it necessary to implement SDL in both the bootloader and the main application, or is it sufficient to add SDL to just one of them?

  2. Documentation or Examples: Are there any resources, guides, or examples that cover this type of SDL integration in projects with a bootloader? I was not able to find any.

Thanks in advance for any advice or insights.

  • Hi llija,

    (+) SAFETI_DIAG_LIB: Guidance on integration SafeTI library with a bootloader - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    There is no special guidance or document for integrating SDL to the application.

    You can refer the existing SDL examples and can do it in the same way.

    You can either use part of the routines or complete SDL based on your application requirements.

    --
    Thanks & regards,
    Jagadish.

  • Hi Jagadish,

    Your answer is quite general, I’ve seen similar answers before on forum, and they don’t address the question in detail. I haven’t found any specific guidance on implementing SDL with a bootloader.

    Could you answer a more specific question about SDL integration? In the bootloader, I have a sys_startup.c file generated by HalCoGen, which is similar to the one in the main project. I’ve implemented sys_startup.c according to the SDL demo example. Do I need to make adjustments in the bootloader's startup routine? Specifically, should I modify or comment out parts related to reading the reset reason, performing initialization functions, or running PBIST in the bootloader?

    Any detailed guidance on handling these parts when SDL is integrated with a bootloader setup would be very helpful.

    Thanks & regards,
    Ilija.

  • Hi Ilija,

    All we have is SDL demos only. 

    Even i will refer the SDL demos codes and answer according to it. My suggestion would be that please refer SDL demo project and create your project in according to it. If you face any difficulty in achieving this then i will work from my side and will provide suggestions.

    --
    Thanks & regards,
    Jagadish.

  • Hi Jagadish,

    I implemented my sys_startup.c file as per the SDL demo application. Everything works fine when the bootloader is not flashed before the main application. However, when the bootloader is present, my main application gets stuck in the following exception handler, with the R14 (undef) register showing 0x00060004, which is not a valid memory address:

    #ifdef __TI_COMPILER_VERSION__
    #pragma INTERRUPT ( _excpt_vec_udef_instr, UDEF)
    void _excpt_vec_udef_instr()
    #endif
    #ifdef __IAR_SYSTEMS_ICC__
    __irq __arm void _excpt_vec_udef_instr()
    #endif
    {
    	while(1);
    
    }

    I traced the issue in debug mode and found that it occurs after the _SL_Kickoff_STC_execution() function is called as part of SL_SelfTest_STC(STC_COMPARE_SELFCHECK, TRUE, &stcSelfTestConfig).

        if (RESET_TYPE_DEBUG == reset_reason)
        {
            /* Make sure that the CPU self-test controller can actually detect a fault inside CPU */
    		stcSelfTestConfig.stcClockDiv		= 0; 			/* STC Clock divider = 1 */
    		stcSelfTestConfig.intervalCount 	= 1; 			/* One interval only */
    		stcSelfTestConfig.restartInterval0 	= TRUE; 		/* Start from interval 0 */
    		stcSelfTestConfig.timeoutCounter 	= 0x1; 	/* Timeout counter*/
    		_SL_HoldNClear_nError();
    
    		/* mask vim interrupts before running STC */
    		vimREG->REQMASKCLR0 = 0xFFFFFFFFu;
    		vimREG->REQMASKCLR1 = 0xFFFFFFFFu;
    		vimREG->REQMASKCLR2 = 0xFFFFFFFFu;
    		vimREG->REQMASKCLR3 = 0xFFFFFFFFu;
    
    		/* ensure no pending ESM GRP2 errors before running STC */
    		if(esmREG->SSR2 == 0u)
    		{
                //! Executes CPU Logic Built-In Self Test using Self-Test Controller
    			SL_SelfTest_STC(STC_COMPARE_SELFCHECK, TRUE, &stcSelfTestConfig);
    		}
    		else
    		{
    			while(1); //ESM Group2 error
    		}
        }
        else
        {
            afterSTC();
        }    
        
    /* USER CODE END */
    }

    Could this issue be related to the reset_reason value? Is it possible that the bootloader alters the reset reason or interferes with the STC initialization?

    Any insights into why this might be happening and whether additional steps are needed in the bootloader or main application to handle this scenario would be greatly appreciated.

    Thanks & regards,

    Ilija.

  • Hi Ilija,

    Could this issue be related to the reset_reason value? Is it possible that the bootloader alters the reset reason or interferes with the STC initialization?

    Actually, bootloader will erase the reset cause, i found this in one of my old threads:

    (+) TMS570LC4357: freertos bootloader application getting problem in I2C - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    Please refer above thread and based on this try to do modifications.

    --
    Thanks & regards,
    Jagadish.

  • Hi Jagadish,

    I have already implemented this in my startup code. I called systemInit(), _coreEnableIrqVicOffset_(), vimInit(), esmInit() before main().

    Here is my application startup code:

    /** @file sys_startup.c 
    *   @brief Startup Source File
    *   @date 11-Dec-2018
    *   @version 04.07.01
    *
    *   This file contains:
    *   - Include Files
    *   - Type Definitions
    *   - External Functions
    *   - VIM RAM Setup
    *   - Startup Routine
    *   .
    *   which are relevant for the Startup.
    */
    
    /* 
    * Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com 
    * 
    * 
    *  Redistribution and use in source and binary forms, with or without 
    *  modification, are permitted provided that the following conditions 
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright 
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the 
    *    documentation and/or other materials provided with the   
    *    distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    */
    
    
    /* USER CODE BEGIN (0) */
    /* USER CODE END */
    
    
    /* Include Files */
    
    #include "sys_common.h"
    #include "system.h"
    #include "sys_vim.h"
    #include "sys_core.h"
    #include "sys_selftest.h"
    #include "esm.h"
    #include "mibspi.h"
    
    #include "errata_SSWF021_45.h"
    /* USER CODE BEGIN (1) */
    #include "sl_api.h"
    #include "sl_priv.h"
    #include "register_readback.h"
    #include "esm_application_callback.h"
    /* USER CODE END */
    
    
    /* USER CODE BEGIN (2) */
    // uint32 ulFlashStartAddr = 0x00000000;
    // uint32 ulFlashEndAddr = 0x0003da08;
    // uint32 *ptrFlashStartAddr = &ulFlashStartAddr;
    // uint32 *ptrFlashEndAddr = &ulFlashEndAddr;
    
    extern uint16_t App_Rst_Src;
    /* USER CODE END */
    
    
    /* External Functions */
    /*SAFETYMCUSW 218 S MR:20.2 <APPROVED> "Functions from library" */
    extern void __TI_auto_init(void);
    /*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(main should be declared by the user)" */
    extern int main(void);
    /*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */
    /*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(Extern declaration present in the library)" */
    extern void exit(int _status);
    
    void afterSTC(void);
    
    /* USER CODE BEGIN (3) */
    #define INCREMENT_PASS_FAIL_COUNTER(x,y)  if ((ST_PASS == (x)) && (TRUE == (y))) {	\
                                                		initSTPassCount++;      		\
                                            		} else {                    		\
                                            			initSTFailCount++;      		\
                                            		}
    
    #pragma SET_DATA_SECTION ()
    volatile uint64 crcAtInit_VIMRAM = 0;
    volatile uint64 crcAtInit_FLASH = 0;
    volatile uint64 crcAtInit_FEE = 0;
    volatile uint64 crcAtInit_StaticRAM = 0;
    uint8 static_ram[8] = {4,2,3,4,5,5,7,9};
    /* USER CODE END */
    void handlePLLLockFail(void);
    /* Startup Routine */
    void _c_int00(void);
    #define PLL_RETRIES 5U
    /* USER CODE BEGIN (4) */
    SL_ResetReason reset_reason;    /* Reset reason */
    SL_ResetReason_XInfo reset_reason_shadow_reg;   /*extended information of the previous reset (using shadow registers)*/
    uint32 			initSTFailCount;	/* Startup self test fail count.. Passed to main */
    uint32 			initSTPassCount; 	/* Startup self test pass count.. Passed to main */
    SL_PBIST_FailInfo           failInfoPBISTSRAM;  /* PBIST Failure information for TCM RAM */
    /* USER CODE END */
    
    #pragma CODE_STATE(_c_int00, 32)
    #pragma INTERRUPT(_c_int00, RESET)
    #pragma WEAK(_c_int00)
    
    /* SourceId : STARTUP_SourceId_001 */
    /* DesignId : STARTUP_DesignId_001 */
    /* Requirements : HL_SR508 */
    void _c_int00(void)
    {    
    /* USER CODE BEGIN (5) */
    	/* NOTE: DO NOT INITIALIZE ANY VARIABLES !! (will cause DABORT because of un-initialized SP) */
    	volatile boolean 			retVal;             /* For function return values */
        SL_STC_Config 				stcSelfTestConfig;  /* STC Configuration */
    
    	extern uint32 ulFlashStartAddr;
    	extern uint32 ulFlashEndAddr;
    
        //! reset source register for debugging, decleraed as register so it wont be reinitialized later by memInit
        register uint32_t rstSrc;
        // #if 0
    
    /* USER CODE END */
    
        /* Initialize Core Registers to avoid CCM Error */
        // _coreInitRegisters_();
    
    /* USER CODE BEGIN (6) */
    // #endif
    //! Change CPU Mode to Supervisor when using bootloader if the bootloader is in the user mode..
    __asm( "    cps #0x13" );
    SL_Init_R4Registers();
    #if 0
    /* USER CODE END */
    
        /* Initialize Stack Pointers */
        _coreInitStackPointer_();
    
    /* USER CODE BEGIN (7) */
    #endif
    SL_Init_StackPointers();
    #if 0
    /* USER CODE END */
    
        /* Enable CPU Event Export */
        /* This allows the CPU to signal any single-bit or double-bit errors detected
         * by its ECC logic for accesses to program flash or data RAM.
         */
        _coreEnableEventBusExport_();
    /* USER CODE BEGIN (9) */
    #endif
    
        /* Enable CPU Event Export */
        /* This allows the CPU to signal any single-bit or double-bit errors detected
         * by its ECC logic for accesses to program flash or data RAM.
         */
        
        _SL_Init_EnableEventExport();
    /* USER CODE END */
    
        /* Enable response to ECC errors indicated by CPU for accesses to flash */
        flashWREG->FEDACCTRL1 = 0x000A060AU;
    
    /* USER CODE BEGIN (10) */
    // #if 0
    /* USER CODE END */
    
        /* Enable CPU ECC checking for ATCM (flash accesses) */
        // _coreEnableFlashEcc_();
    	
    
    /* USER CODE BEGIN (11) */
    // #endif
        /*enable the flash SECDED logic in order to capture any ECC errors*/
        SL_Init_ECCFlash(10, FLASHECC_DEFAULT); /* Enable Flash ECC */
    
        // _SL_HoldNClear_nError();
        // Read reset reason
        reset_reason = SL_Init_ResetReason();
    
        // reset_reason = RESET_TYPE_WATCHDOG;
    
        // read reset shadow registers
        retVal = SL_Init_ResetReason_XInfo(&reset_reason_shadow_reg);
    
        /* Workaround for Errata CORTEXR4 66 */
        _errata_CORTEXR4_66_();
    
        /* Workaround for Errata CORTEXR4 57 */
        _errata_CORTEXR4_57_();
    
    #if 0
    /* USER CODE END */
    
            /* Workaround for Errata CORTEXR4 66 */
            _errata_CORTEXR4_66_();
        
            /* Workaround for Errata CORTEXR4 57 */ 
            _errata_CORTEXR4_57_();
    
        /* Reset handler: the following instructions read from the system exception status register
         * to identify the cause of the CPU reset.
         */
    
        /* check for power-on reset condition */
        /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
        if ((SYS_EXCEPTION & POWERON_RESET) != 0U)
        {		
    /* USER CODE BEGIN (12) */
    #endif
        if (RESET_TYPE_POWERON == reset_reason)
        { // !ovo handlePLLLockFail() nema u sdl_demo        
    /* USER CODE END */
            /* Add condition to check whether PLL can be started successfully */
            if (_errata_SSWF021_45_pll1(PLL_RETRIES) != 0U)
            {
                /* Put system in a safe state */
    			handlePLLLockFail();
            }
            /* clear all reset status flags */
            SYS_EXCEPTION = 0xFFFFU;
    
    /* USER CODE BEGIN (13) */
    /* USER CODE END */
    /* USER CODE BEGIN (14) */
    /* USER CODE END */
    /* USER CODE BEGIN (15) */
    #if 0
    /* USER CODE END */
          /* continue with normal start-up sequence */
        }
        /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
        else if ((SYS_EXCEPTION & OSC_FAILURE_RESET) != 0U)
        {
            /* Reset caused due to oscillator failure.
            Add user code here to handle oscillator failure */
    
    /* USER CODE BEGIN (16) */
    #endif
        }
        else if (RESET_TYPE_OSC_FAILURE == reset_reason)
        {
            while (1)
            {
                /* code */
            }
            
    #if 0
    /* USER CODE END */
        }
        /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
        else if ((SYS_EXCEPTION & WATCHDOG_RESET) !=0U)
        {
            /* Reset caused due 
             *  1) windowed watchdog violation - Add user code here to handle watchdog violation.
             *  2) ICEPICK Reset - After loading code via CCS / System Reset through CCS
             */
            /* Check the WatchDog Status register */
            if(WATCHDOG_STATUS != 0U)
            {
                /* Add user code here to handle watchdog violation. */ 
    /* USER CODE BEGIN (17) */
    #endif
        }
        else if (RESET_TYPE_WATCHDOG == reset_reason)
        {
            /* Reset caused due 
             *  1) windowed watchdog violation - Add user code here to handle watchdog violation.
             *  2) ICEPICK Reset - After loading code via CCS / System Reset through CCS
             */
            /* Check the WatchDog Status register */
            if(WATCHDOG_STATUS != 0U)
            {
                /* Add user code here to handle watchdog violation. */ 
    /* USER CODE END */
    
                /* Clear the Watchdog reset flag in Exception Status register */ 
                SYS_EXCEPTION = WATCHDOG_RESET;
            
    /* USER CODE BEGIN (18) */
    /* USER CODE END */
            }
            else
            {
                /* Clear the ICEPICK reset flag in Exception Status register */ 
                SYS_EXCEPTION = ICEPICK_RESET;
    /* USER CODE BEGIN (19) */
    #if 0
    /* USER CODE END */
    		}
        }
        /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
        else if ((SYS_EXCEPTION & CPU_RESET) !=0U)
        {
            /* Reset caused due to CPU reset.
            CPU reset can be caused by CPU self-test completion, or
            by toggling the "CPU RESET" bit of the CPU Reset Control Register. */
    
    /* USER CODE BEGIN (20) */
    #endif
            }
        }
        else if (RESET_TYPE_CPU == reset_reason)
        {
            /* Reset caused due to CPU reset.
    		CPU reset can be caused by CPU self-test completion, or
    		by toggling the "CPU RESET" bit of the CPU Reset Control Register. */
    
    		/*********NOTE*********/
        	/*Call to CPU Self-Test via HALCoGen API has to be replaced with SafeTI Lib API
    		 * everytime HALCoGen code is generated (since it gets over written) */
    /* USER CODE END */
    
            /* clear all reset status flags */
            SYS_EXCEPTION = CPU_RESET;
    
            /* reset could be caused by stcSelfCheck run or by an actual CPU self-test run */
            
            /* check if this was an stcSelfCheck run */
            if ((stcREG->STCSCSCR & 0xFU) == 0xAU)            
            {
                /* check if the self-test fail bit is set */
                if ((stcREG->STCGSTAT & 0x3U) != 0x3U)
                {
                    /* STC self-check has failed */
                    stcSelfCheckFail();                        
                }
                /* STC self-check has passed */
                else                                        
                {
                    /* clear self-check mode */
                    stcREG->STCSCSCR = 0x05U;                
                    
                    /* clear STC global status flags */
                    stcREG->STCGSTAT = 0x3U;                
                    
                    /* clear ESM group1 channel 27 status flag */
                    esmREG->SR1[0U] = 0x08000000U;        
                    
                    /* Start CPU Self-Test */
                    cpuSelfTest(STC_INTERVAL, STC_MAX_TIMEOUT, TRUE);                            
                }
            }
            /* CPU reset caused by CPU self-test completion */
            else if ((stcREG->STCGSTAT & 0x1U) == 0x1U)        
            {
                /* Self-Test Fail flag is set */
                if ((stcREG->STCGSTAT & 0x2U) == 0x2U)        
                {
                    /* Call CPU self-test failure handler */
                    cpuSelfTestFail();                    
                }
                /* CPU self-test completed successfully */
                else                                        
                {
                    /* clear STC global status flag */
                    stcREG->STCGSTAT = 0x1U;  
                    
                    /* Continue start-up sequence after CPU STC completed */
                    afterSTC();                                
                }
            }
            /* CPU reset caused by software writing to CPU RESET bit */
            else                                            
            {
                /* Add custom routine here to handle the case where software causes CPU reset */
            }
    /* USER CODE BEGIN (21) */
    #if 0
    /* USER CODE END */
    
        }
        /*SAFETYMCUSW 139 S MR:13.7 <APPROVED> "Hardware status bit read check" */
        else if ((SYS_EXCEPTION & SW_RESET) != 0U)
        {
            /* Reset caused due to software reset.
            Add user code to handle software reset. */
    		
    /* USER CODE BEGIN (22) */
    #endif
        }
        else if (RESET_TYPE_SWRST == reset_reason)
        {
            // while (1)
            // {
            //     /* code */
            // }
            
        
    /* USER CODE END */
    	}
        else
        {
            /* Reset caused by nRST being driven low externally.
            Add user code to handle external reset. */
    
    /* USER CODE BEGIN (23) */
    /* USER CODE END */
    	}
    
        /* Check if there were ESM group3 errors during power-up.
         * These could occur during eFuse auto-load or during reads from flash OTP
         * during power-up. Device operation is not reliable and not recommended
         * in this case.
         * An ESM group3 error only drives the nERROR pin low. An external circuit
         * that monitors the nERROR pin must take the appropriate action to ensure that
         * the system is placed in a safe state, as determined by the application.
         */
        if ((esmREG->SR1[2]) != 0U)
        {
    /* USER CODE BEGIN (24) */
    /* USER CODE END */
        /*SAFETYMCUSW 5 C MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
        /*SAFETYMCUSW 26 S MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
        /*SAFETYMCUSW 28 D MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
            for(;;)
            { 
            }/* Wait */                 
    /* USER CODE BEGIN (25) */
    /* USER CODE END */
        }
    
    /* USER CODE BEGIN (26) */
    #if 0
    /* USER CODE END */
    
        /* Initialize System - Clock, Flash settings with Efuse self check */
        systemInit();
        
        /* Workaround for Errata PBIST#4 */
        errata_PBIST_4();
    	
        /* Run a diagnostic check on the memory self-test controller.
         * This function chooses a RAM test algorithm and runs it on an on-chip ROM.
         * The memory self-test is expected to fail. The function ensures that the PBIST controller
         * is capable of detecting and indicating a memory self-test failure.
         */
        pbistSelfCheck();	
    	
    	/* Run PBIST on STC ROM */
        pbistRun((uint32)STC_ROM_PBIST_RAM_GROUP,
                 ((uint32)PBIST_TripleReadSlow | (uint32)PBIST_TripleReadFast));
        
        /* Wait for PBIST for STC ROM to be completed */
        /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
        while(pbistIsTestCompleted() != TRUE)
        { 
        }/* Wait */ 
        
        /* Check if PBIST on STC ROM passed the self-test */
        if( pbistIsTestPassed() != TRUE)
        {
            /* PBIST and STC ROM failed the self-test.
             * Need custom handler to check the memory failure
             * and to take the appropriate next step.
             */
             
            pbistFail();
    
        }   
    	
        /* Disable PBIST clocks and disable memory self-test mode */
        pbistStop();
    
    	/* Run PBIST on PBIST ROM */
        pbistRun((uint32)PBIST_ROM_PBIST_RAM_GROUP,
                 ((uint32)PBIST_TripleReadSlow | (uint32)PBIST_TripleReadFast));
        
        /* Wait for PBIST for PBIST ROM to be completed */
        /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
        while(pbistIsTestCompleted() != TRUE)
        { 
        }/* Wait */ 
        
        /* Check if PBIST ROM passed the self-test */
        if( pbistIsTestPassed() != TRUE)
        {
            /* PBIST and STC ROM failed the self-test.
             * Need custom handler to check the memory failure
             * and to take the appropriate next step.
             */
             
            pbistFail();
    
        } 
    	
        /* Disable PBIST clocks and disable memory self-test mode */
        pbistStop();	
    /* USER CODE BEGIN (27) */
    #endif
    /* Initialize System - Clock, Flash settings with Efuse self check */
        systemInit();
    
        /* Workaround for Errata PBIST#4 */
        errata_PBIST_4();
    
        /* Run a diagnostic check on the memory self-test controller.
         * This function chooses a RAM test algorithm and runs it on an on-chip ROM.
         * The memory self-test is expected to fail. The function ensures that the PBIST controller
         * is capable of detecting and indicating a memory self-test failure.
         */
        pbistSelfCheck();
    
        _SL_HoldNClear_nError();
    
    	/* Run PBIST on PBIST ROM */
    	retVal = SL_SelfTest_PBIST( PBIST_EXECUTE,
    								PBIST_RAMGROUP_02_STC_ROM,
    								PBISTALGO_TRIPLE_READ_SLOW_READ|PBISTALGO_TRIPLE_READ_FAST_READ);
    	while (TRUE != SL_SelfTest_WaitCompletion_PBIST());
    	retVal = SL_SelfTest_Status_PBIST(&failInfoPBISTSRAM);
    	if (failInfoPBISTSRAM.stResult == ST_PASS) {
    		initSTPassCount++;
    	} else {
    		initSTFailCount++;
    		for(;;)
    		{
    		}/* Wait */
    	}
    
    	/* Disable PBIST clocks and disable memory self-test mode */
    	SL_SelfTest_PBIST_StopExec();
    
        /* Run PBIST on STC ROM */
        retVal = SL_SelfTest_PBIST( PBIST_EXECUTE,
    								PBIST_RAMGROUP_01_PBIST_ROM,
                                    PBISTALGO_TRIPLE_READ_SLOW_READ|PBISTALGO_TRIPLE_READ_FAST_READ);
        while (TRUE != SL_SelfTest_WaitCompletion_PBIST());
        retVal = SL_SelfTest_Status_PBIST(&failInfoPBISTSRAM);
        if (failInfoPBISTSRAM.stResult == ST_PASS) {
        	initSTPassCount++;
        } else {
        	initSTFailCount++;
        	for(;;)
        	{
        	}/* Wait */
        }
    
    	/* Disable PBIST clocks and disable memory self-test mode */
    	SL_SelfTest_PBIST_StopExec();
    
    // ! cannot be run in debug mode
    
    #if 0
    /* USER CODE END */
    
        /* Make sure that the CPU self-test controller can actually detect a fault inside CPU */
        stcSelfCheck();
    
    /* USER CODE BEGIN (28) */
    #endif
        /*At the end of the STC execution a CPU reset is issued by the STC controller.
        So the application startup must ensure that the STC is not-executed when reset type 
        is RESET_TYPE_CPU & when the debugger is connected*/
    
        if (RESET_TYPE_DEBUG != reset_reason)
        {
            /* Make sure that the CPU self-test controller can actually detect a fault inside CPU */
    		stcSelfTestConfig.stcClockDiv		= 0; 			/* STC Clock divider = 1 */
    		stcSelfTestConfig.intervalCount 	= 1; 			/* One interval only */
    		stcSelfTestConfig.restartInterval0 	= TRUE; 		/* Start from interval 0 */
    		stcSelfTestConfig.timeoutCounter 	= 0x1; 	/* Timeout counter*/
    		_SL_HoldNClear_nError();
    
    		/* mask vim interrupts before running STC */
    		vimREG->REQMASKCLR0 = 0xFFFFFFFFu;
    		vimREG->REQMASKCLR1 = 0xFFFFFFFFu;
    		vimREG->REQMASKCLR2 = 0xFFFFFFFFu;
    		vimREG->REQMASKCLR3 = 0xFFFFFFFFu;
    
    		/* ensure no pending ESM GRP2 errors before running STC */
    		if(esmREG->SSR2 == 0u)
    		{
                //! Executes CPU Logic Built-In Self Test using Self-Test Controller
    			SL_SelfTest_STC(STC_COMPARE_SELFCHECK, TRUE, &stcSelfTestConfig);
    		}
    		else
    		{
    			while(1); //ESM Group2 error
    		}
        }
        else
        {
            afterSTC();
        }    
        
    /* USER CODE END */
    }
    
    void afterSTC(void)
    {
    /* USER CODE BEGIN (29) */
        SL_CCMR4F_FailInfo  failInfoCCMR4F; /* CCMR4F Self Test fail info */
        
        volatile boolean 			retVal;             /* For function return values */
        SL_SelfTest_Result          failInfoFlash;      /* Flash Self test failure information */
        SL_SelfTest_Result          failInfoTCMRAM;     /* TCM RAM Failure  information */
        SL_PBIST_FailInfo           failInfoPBISTOthers;/* PBIST Failure information for non-TCM memories */
        SL_PSCON_FailInfo           failInfoPSCON;      /* PSCON failure information */ //! ovo nema za RM44
        SL_EFuse_Config             stConfigEFuse;      /* EFuse self test configuration */
    
        extern uint32               ulFlashStartAddr;   /* Used for Flash CRC Calculation */
        extern uint32               ulFlashEndAddr;     /* Used for Flash CRC Calculation */
    /* USER CODE END */
    
        /* Make sure that CCM-R4F is working as expected.
         * This function puts the CCM-R4F module through its self-test modes.
         * It ensures that the CCM-R4F is indeed capable of detecting a CPU mismatch,
         * and is also capable of indicating a mismatch error to the ESM.
         */
        
        // ccmSelfCheck();
    
    /* USER CODE BEGIN (30) */
    /* Make sure that CCM-R4F is working as expected.
    	 * This function puts the CCM-R4F module through its self-test modes.
    	 * It ensures that the CCM-R4F is indeed capable of detecting a CPU mismatch,
    	 * and is also capable of indicating a mismatch error to the ESM.
    	 */
    	/* Can be enabled when in release */
    #if 0 
        //! Executes self-tests on Core Compare Module (CCM). 
    	/* With debugger connected, CCM is disabled so do not run when debugger is connected */
    	if (RESET_TYPE_DEBUG != reset_reason)
    	{
    		/* Try CCMR4F Fault Injection */
    		retVal = SL_SelfTest_CCMR4F(CCMR4F_SELF_TEST, TRUE, &failInfoCCMR4F);
    //		INCREMENT_PASS_FAIL_COUNTER(failInfoCCMR4F.stResult, retVal);
    
    		retVal = SL_SelfTest_CCMR4F(CCMR4F_ERROR_FORCING_TEST, TRUE, &failInfoCCMR4F);
    //		INCREMENT_PASS_FAIL_COUNTER(failInfoCCMR4F.stResult, retVal);
    
    		retVal = SL_SelfTest_CCMR4F(CCMR4F_SELF_TEST_ERROR_FORCING, TRUE, &failInfoCCMR4F);
    //		INCREMENT_PASS_FAIL_COUNTER(failInfoCCMR4F.stResult, retVal);
    	}
    #endif
    /* USER CODE END */
    
    /* USER CODE BEGIN (31) */
    
    /* USER CODE END */
    
        /* Disable RAM ECC before doing PBIST for Main RAM */
        _coreDisableRamEcc_();
        
        /* Run PBIST on CPU RAM.
         * The PBIST controller needs to be configured separately for single-port and dual-port SRAMs.
         * The CPU RAM is a single-port memory. The actual "RAM Group" for all on-chip SRAMs is defined in the
         * device datasheet.
         */
        pbistRun(0x00100020U, /* ESRAM Single Port PBIST */
                 (uint32)PBIST_March13N_SP);
    
    /* USER CODE BEGIN (32) */
    /* NOTE: Not recommended to conduct pbist test on SRAM - can cause race condition between corruption
     * of stack pointer and return from function call */
    
    #if 0
    /* USER CODE END */
    
        /* Wait for PBIST for CPU RAM to be completed */
        /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
        while(pbistIsTestCompleted() != TRUE)
        { 
        }/* Wait */                 
        
    
    /* USER CODE BEGIN (33) */
    #endif
    
        while (TRUE != SL_SelfTest_WaitCompletion_PBIST())
        {
            /* code */
        }
    #if 0
    /* USER CODE END */
        
        /* Check if CPU RAM passed the self-test */
        if( pbistIsTestPassed() != TRUE)
        {
            /* CPU RAM failed the self-test.
             * Need custom handler to check the memory failure
             * and to take the appropriate next step.
             */
    /* USER CODE BEGIN (34) */
    #endif
        
        /* Get SRAM PBIST Status */
    	SL_SelfTest_Status_PBIST(&failInfoPBISTSRAM);
    #if 0
    /* USER CODE END */
             
            pbistFail();
            
    /* USER CODE BEGIN (35) */
    #endif
    		if (failInfoPBISTSRAM.stResult == ST_PASS) {
    			initSTPassCount++;
    		} else {
    			initSTFailCount++;
    			   for(;;)
    			   {
    			   }/* Wait */
    /* USER CODE END */
        }
    
    /* USER CODE BEGIN (36) */
    #if 0
    /* USER CODE END */
    
        /* Disable PBIST clocks and disable memory self-test mode */
        pbistStop();
    
        
    /* USER CODE BEGIN (37) */
    #endif
        /* Disable PBIST clocks and disable memory self-test mode */
        SL_SelfTest_PBIST_StopExec();
    #if 0
    /* USER CODE END */
    
    
        /* Initialize CPU RAM.
         * This function uses the system module's hardware for auto-initialization of memories and their
         * associated protection schemes. The CPU RAM is initialized by setting bit 0 of the MSIENA register.
         * Hence the value 0x1 passed to the function.
         * This function will initialize the entire CPU RAM and the corresponding ECC locations.
         */
        memoryInit(0x1U);
    
    /* USER CODE BEGIN (38) */
    #endif
    /* Initialize CPU RAM.
    	 * This function uses the system module's hardware for auto-initialization of memories and their
    	 * associated protection schemes. The CPU RAM is initialized by setting bit 0 of the MSIENA register.
    	 * Hence the value 0x1 passed to the function.
    	 * This function will initialize the entire CPU RAM and the corresponding ECC locations.
    	 */
    
    	SL_Init_Memory(RAMTYPE_RAM);
    #if 0
    /* USER CODE END */
        
        /* Enable ECC checking for TCRAM accesses.
         * This function enables the CPU's ECC logic for accesses to B0TCM and B1TCM.
         */
        _coreEnableRamEcc_();
    
    /* USER CODE BEGIN (39) */
    #endif
        SL_Init_ECCTCMRAM(10, TRUE);       /* Enable TCM RAM ECC */
    #if 0
    /* USER CODE END */
    
        /* Start PBIST on all dual-port memories */
        /* NOTE : Please Refer DEVICE DATASHEET for the list of Supported Dual port Memories.
           PBIST test performed only on the user selected memories in HALCoGen's GUI SAFETY INIT tab.
         */
        pbistRun(  (uint32)0x00000000U    /* EMAC RAM */
                 | (uint32)0x00000000U    /* USB RAM */  
                 | (uint32)0x00000800U    /* DMA RAM */
                 | (uint32)0x00000200U    /* VIM RAM */
                 | (uint32)0x00000040U    /* MIBSPI1 RAM */
                 | (uint32)0x00000080U    /* MIBSPI3 RAM */
                 | (uint32)0x00000000U    /* MIBSPI5 RAM */
                 | (uint32)0x00000004U    /* CAN1 RAM */
                 | (uint32)0x00000008U    /* CAN2 RAM */
                 | (uint32)0x00000000U    /* CAN3 RAM */
                 | (uint32)0x00000400U    /* ADC1 RAM */
                 | (uint32)0x00020000U    /* ADC2 RAM */
                 | (uint32)0x00001000U    /* HET1 RAM */
                 | (uint32)0x00040000U    /* HET2 RAM */
                 | (uint32)0x00002000U    /* HTU1 RAM */
                 | (uint32)0x00080000U    /* HTU2 RAM */
                 | (uint32)0x00000000U    /* RTP RAM */
                 | (uint32)0x00000000U    /* FRAY RAM */
                 ,(uint32) PBIST_March13N_DP);
    
    /* USER CODE BEGIN (40) */
    #endif
        /* Execute PBIST tests on required dual-port memories */
        retVal = SL_SelfTest_PBIST( PBIST_EXECUTE,
                                    (PBIST_RAMGROUP_12_DMA 	  |
                                    PBIST_RAMGROUP_07_MIBSPI1 |
                                    PBIST_RAMGROUP_08_MIBSPI3 |
                                    PBIST_RAMGROUP_10_VIM     |
    								PBIST_RAMGROUP_03_DCAN1   |
    								PBIST_RAMGROUP_04_DCAN2   |
                                    PBIST_RAMGROUP_11_MIBADC1 |
                                    PBIST_RAMGROUP_18_MIBADC2 |
    								PBIST_RAMGROUP_13_N2HET1  |
    								PBIST_RAMGROUP_19_N2HET2  |
    								PBIST_RAMGROUP_14_HETTU1  |
    								PBIST_RAMGROUP_20_HETTU2
    								),
                                    PBISTALGO_MARCH13N_RED_2PORT);
    
    #if 0
    /* USER CODE END */
    
        /* Test the CPU ECC mechanism for RAM accesses.
         * The checkBxRAMECC functions cause deliberate single-bit and double-bit errors in TCRAM accesses
         * by corrupting 1 or 2 bits in the ECC. Reading from the TCRAM location with a 2-bit error
         * in the ECC causes a data abort exception. The data abort handler is written to look for
         * deliberately caused exception and to return the code execution to the instruction
         * following the one that caused the abort.
         */
        checkRAMECC();
    
    /* USER CODE BEGIN (41) */
    #endif
        if (SL_ESM_nERROR_Active() == TRUE)
        {
            while (1)
            {
                /* code */
            }
            
        }
        vimInit();
    
        // Execute diagnostics test on TCM RAM
        
        retVal = SL_SelfTest_SRAM(SRAM_PAR_ADDR_CTRL_SELF_TEST, TRUE, &failInfoTCMRAM);
        INCREMENT_PASS_FAIL_COUNTER(failInfoTCMRAM, retVal);
    
        /* Run 1Bit ECC test on TCM RAM */
        retVal = SL_SelfTest_SRAM(SRAM_ECC_ERROR_FORCING_1BIT, TRUE, &failInfoTCMRAM);
        INCREMENT_PASS_FAIL_COUNTER(failInfoTCMRAM, retVal);
    
        /* Run 1Bit ECC error profiling test on TCM RAM */
       retVal = SL_SelfTest_SRAM(SRAM_ECC_ERROR_PROFILING, TRUE, &failInfoTCMRAM);
       INCREMENT_PASS_FAIL_COUNTER(failInfoTCMRAM, retVal);
    
     retVal = SL_SelfTest_SRAM(SRAM_ECC_ERROR_FORCING_2BIT, TRUE, &failInfoTCMRAM);
    //    INCREMENT_PASS_FAIL_COUNTER(failInfoTCMRAM, retVal);
    
    //    if (failInfoTCMRAM == ST_FAIL)
    //    {
    //     while(1);
    //    }
       
    #if 0
    /* USER CODE END */
    
        /* Test the CPU ECC mechanism for Flash accesses.
         * The checkFlashECC function uses the flash interface module's diagnostic mode 7
         * to create single-bit and double-bit errors in CPU accesses to the flash. A double-bit
         * error on reading from flash causes a data abort exception.
         * The data abort handler is written to look for deliberately caused exception and
         * to return the code execution to the instruction following the one that was aborted.
         *
         */
        checkFlashECC();
        flashWREG->FDIAGCTRL = 0x000A0007U;                    /* disable flash diagnostic mode */
    
    /* USER CODE BEGIN (42) */
    #endif
    
    // #if 0
    
        // Execute diagnostic tests on F021 Flash
    
    	/* Run Diagmode 1 */
    	retVal = SL_SelfTest_FEE(FEE_ECC_DATA_CORR_MODE, TRUE, &failInfoFlash);
    	// INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
    
    	/* Run 1 bit selftest */
    	retVal = SL_SelfTest_FEE(FEE_ECC_TEST_MODE_1BIT, TRUE, &failInfoFlash);
    	// INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
    
    	/* Run 2 bit selftest */
    	retVal = SL_SelfTest_FEE(FEE_ECC_TEST_MODE_2BIT, TRUE, &failInfoFlash);
    	// INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
    
    	/* Run Diagmode 2 */
    	retVal = SL_SelfTest_FEE(FEE_ECC_SYN_REPORT_MODE, TRUE, &failInfoFlash);
    	// INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
    
    	/* Run Diagmode 3 */
    	retVal = SL_SelfTest_FEE(FEE_ECC_MALFUNCTION_MODE1, TRUE, &failInfoFlash);
    	// INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
    
    	/* Run Diagmode 4 */
    	retVal = SL_SelfTest_FEE(FEE_ECC_MALFUNCTION_MODE2, TRUE, &failInfoFlash);
    	// INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
    
        /* Run 1Bit ECC test on Flash */
        retVal = SL_SelfTest_Flash(FLASH_ECC_TEST_MODE_1BIT, TRUE, &failInfoFlash);
        // INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
    
        //! check why this test fail
        /* Run 2Bit ECC test on Flash */
        // retVal = SL_SelfTest_Flash(FLASH_ECC_TEST_MODE_2BIT, TRUE, &failInfoFlash);
        // INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
    
        // if (failInfoFlash == ST_FAIL)
        // {
        //     while(1);
        // }
        
    
    // #endif
    
    // #if 0
       /* Run Address tag mode test on Flash */
       //! this cause abort is commented in SDL_demo too
       // diasble pipelining
        // sl_flashWREG->FRDCNTL &= (~0x00000001);
      
        // retVal = SL_SelfTest_Flash(FLASH_ECC_ADDR_TAG_REG_MODE, TRUE, &failInfoFlash);
        // INCREMENT_PASS_FAIL_COUNTER(failInfoFlash, retVal);
        
        // enable pipelining
        // sl_flashWREG->FRDCNTL |= (~0x00000001);
    // #endif
    /* USER CODE END */
    
    /* USER CODE BEGIN (43) */
    #if 0
    /* USER CODE END */
    
        /* Wait for PBIST for CPU RAM to be completed */
        /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
        while(pbistIsTestCompleted() != TRUE)
        { 
        }/* Wait */                 
        
    
    /* USER CODE BEGIN (44) */
    #endif
        
        while (TRUE != SL_SelfTest_WaitCompletion_PBIST());
    	SL_SelfTest_Status_PBIST(&failInfoPBISTOthers);
    
    #if 0
    /* USER CODE END */
    
        /* Check if CPU RAM passed the self-test */
        if( pbistIsTestPassed() != TRUE)
        {
    
    /* USER CODE BEGIN (45) */
    /* USER CODE END */
    
            /* CPU RAM failed the self-test.
             * Need custom handler to check the memory failure
             * and to take the appropriate next step.
             */
    /* USER CODE BEGIN (46) */
    /* USER CODE END */
             
            pbistFail();
            
    /* USER CODE BEGIN (47) */
    /* USER CODE END */
        }
    
    /* USER CODE BEGIN (48) */
    #endif
    	/* Check the PBIST status and if there is a failure then wait */
    	if (failInfoPBISTOthers.stResult == ST_PASS) {
    		initSTPassCount++;
    	} else {
    		initSTFailCount++;
    		   for(;;)
    		   {
    		   } //Wait
    	}
    #if 0
    /* USER CODE END */
    
        /* Disable PBIST clocks and disable memory self-test mode */
        pbistStop();
        
    /* USER CODE BEGIN (55) */
    #endif
    	/* Disable PBIST clocks and disable memory self-test mode */
    	SL_SelfTest_PBIST_StopExec();
    /* USER CODE END */
    
        /* Release the MibSPI1 modules from local reset.
         * This will cause the MibSPI1 RAMs to get initialized along with the parity memory.
         */
         mibspiREG1->GCR0 = 0x1U;
         
        /* Release the MibSPI3 modules from local reset.
         * This will cause the MibSPI3 RAMs to get initialized along with the parity memory.
         */
        mibspiREG3->GCR0 = 0x1U;
        
    /* USER CODE BEGIN (56) */
        // vimInit();
    /* USER CODE END */
    
        /* Enable parity on selected RAMs */
        enableParity();
        
        /* Initialize all on-chip SRAMs except for MibSPIx RAMs
         * The MibSPIx modules have their own auto-initialization mechanism which is triggered
         * as soon as the modules are brought out of local reset.
         */
        /* The system module auto-init will hang on the MibSPI RAM if the module is still in local reset.
         */
        /* NOTE : Please Refer DEVICE DATASHEET for the list of Supported Memories and their channel numbers.
                  Memory Initialization is perfomed only on the user selected memories in HALCoGen's GUI SAFETY INIT tab.
         */
        memoryInit( (uint32)((uint32)1U << 1U)    /* DMA RAM */
                  | (uint32)((uint32)1U << 2U)    /* VIM RAM */
                  | (uint32)((uint32)1U << 5U)    /* CAN1 RAM */
                  | (uint32)((uint32)1U << 6U)    /* CAN2 RAM */
                  | (uint32)((uint32)0U << 10U)   /* CAN3 RAM */
                  | (uint32)((uint32)1U << 8U)    /* ADC1 RAM */
                  | (uint32)((uint32)1U << 14U)   /* ADC2 RAM */
                  | (uint32)((uint32)1U << 3U)    /* HET1 RAM */
                  | (uint32)((uint32)1U << 4U)    /* HTU1 RAM */
                  | (uint32)((uint32)1U << 15U)   /* HET2 RAM */
                  | (uint32)((uint32)1U << 16U)   /* HTU2 RAM */
                  );
    
        /* Disable parity */
        disableParity();
        
        /* Test the parity protection mechanism for peripheral RAMs
           NOTE : Please Refer DEVICE DATASHEET for the list of Supported Memories with parity.
                     Parity Self check is perfomed only on the user selected memories in HALCoGen's GUI SAFETY INIT tab.
        */
    
    /* USER CODE BEGIN (57) */
    /* USER CODE END */
         
        het1ParityCheck();
        
    /* USER CODE BEGIN (58) */
    /* USER CODE END */
    
        htu1ParityCheck();
        
    /* USER CODE BEGIN (59) */
    /* USER CODE END */
    
        het2ParityCheck();
        
    /* USER CODE BEGIN (60) */
    /* USER CODE END */
    
        htu2ParityCheck();
        
    /* USER CODE BEGIN (61) */
    /* USER CODE END */
    
        adc1ParityCheck();
        
    /* USER CODE BEGIN (62) */
    /* USER CODE END */
    
        adc2ParityCheck();
        
    /* USER CODE BEGIN (63) */
    /* USER CODE END */
    
        can1ParityCheck();
        
    /* USER CODE BEGIN (64) */
    /* USER CODE END */
    
        can2ParityCheck();
        
    /* USER CODE BEGIN (66) */
    /* USER CODE END */
    
        vimParityCheck();
        
    /* USER CODE BEGIN (67) */
    /* USER CODE END */
    
        dmaParityCheck();
    
    
    /* USER CODE BEGIN (68) */
    /* USER CODE END */
    
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
        while ((mibspiREG1->FLG & 0x01000000U) == 0x01000000U)
        { 
        }/* Wait */                 
        /* wait for MibSPI1 RAM to complete initialization */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
        while ((mibspiREG3->FLG & 0x01000000U) == 0x01000000U)
        { 
        }/* Wait */                 
        /* wait for MibSPI3 RAM to complete initialization */ 
    
    /* USER CODE BEGIN (69) */
    /* USER CODE END */
    
        mibspi1ParityCheck();
        
    /* USER CODE BEGIN (70) */
    /* USER CODE END */
    
        mibspi3ParityCheck();
        
    
    /* USER CODE BEGIN (72) */
    /* USER CODE END */
        
        /* Enable IRQ offset via Vic controller */
        _coreEnableIrqVicOffset_();
        
    
    /* USER CODE BEGIN (73) */
    /* USER CODE END */
    
        /* Initialize VIM table */
        vimInit();    
    
    /* USER CODE BEGIN (74) */
    /* USER CODE END */
    
        /* Configure system response to error conditions signaled to the ESM group1 */
        /* This function can be configured from the ESM tab of HALCoGen */
        esmInit();
        /* initialize copy table */
        __TI_auto_init();
    /* USER CODE BEGIN (75) */
        // checkPLL1Slip();
        // checkClockMonitor();
    
        // #if 0
        /* Run EFuse self tests */
        stConfigEFuse.numPatterns      = 600u;
        stConfigEFuse.seedSignature    = 0x5362F97Fu;
        stConfigEFuse.failInfo.stResult= ST_FAIL;
        stConfigEFuse.failInfo.failInfo= EFUSE_ERROR_NONE;
       
        // retVal = SL_SelfTest_EFuse(EFUSE_SELF_TEST_STUCK_AT_ZERO, TRUE, &stConfigEFuse);
        // INCREMENT_PASS_FAIL_COUNTER(stConfigEFuse.failInfo.stResult, retVal);
    
        // retVal = SL_SelfTest_EFuse(EFUSE_SELF_TEST_ECC, TRUE, &stConfigEFuse);
        // while (TRUE != SL_SelfTest_Status_EFuse(&stConfigEFuse.failInfo));
        // INCREMENT_PASS_FAIL_COUNTER(stConfigEFuse.failInfo.stResult, retVal);
    
     
        /* Run RAD Self tests on TCMRAM */
        // retVal = SL_SelfTest_SRAM(SRAM_RADECODE_DIAGNOSTICS, TRUE, &failInfoTCMRAM);
        // INCREMENT_PASS_FAIL_COUNTER(failInfoTCMRAM, retVal);
    
       
        // retVal = SL_SelfTest_SRAM(SRAM_PAR_ADDR_CTRL_SELF_TEST, TRUE, &failInfoTCMRAM);
    	// INCREMENT_PASS_FAIL_COUNTER(failInfoTCMRAM, retVal);
    
    
        //! commented staf that say remove this later
    	/* Enable parity checking for dma (for now - remove this later) */
    	dmaEnableParityCheck();
    
    	/* Enable parity checking for vim (for now - remove this later) */
    	sl_vimParREG->PARCTL = 0xAU;
    
    	hetInit();
        /* Turn HET off (for now - remove this later) */
        sl_hetREG1->GCR &= (~(uint32)0x1U);
        sl_hetREG2->GCR &= (~(uint32)0x1U);
    
    	/* Enable parity checking for htu (for now - remove this later) */
        sl_htuREG1->PCR = 0xAU;
        sl_htuREG2->PCR = 0xAU;
    
        /* Enable htu (for now - remove this later) */
        sl_htuREG1->GC |= (uint32)0x10000u;
        sl_htuREG2->GC |= (uint32)0x10000u;
    
    		mibspiInit();
    		canInit();
    		// spiInit();
    		// gioInit();
    		// sciInit();
    		adcInit();
    
        /* Configure system response to error conditions signaled to the ESM group1 */
        /* This function can be configured from the ESM tab of HALCoGen */
        esmInit();
        /* initialize copy table */
        __TI_auto_init();
    
        SL_ESM_Init(ESM_ApplicationCallback);
    	crcAtInit_VIMRAM = SL_CRC_Calculate(((uint64 *)0xFFF82000), 256);
    	crcAtInit_FEE = SL_CRC_Calculate(((uint64 *)0xF0200000), 8);
    
        crcAtInit_FLASH = SL_CRC_Calculate((uint64 *)((uint32)&ulFlashStartAddr), ((((uint32)&ulFlashEndAddr)-((uint32)&ulFlashStartAddr)) >> 3));
        crcAtInit_StaticRAM = SL_CRC_Calculate((uint64*)static_ram,1);    /* enable the below functions only if profiling is ebnabled*/
        _enable_interrupt_();
    
        Reg_Read_Compare(PMM,BASELINE);   
        Reg_Read_Compare(DCC1,REBASELINE);
        Reg_Read_Compare(DCC2,REBASELINE);
        Reg_Read_Compare(SYSTEM,REBASELINE);
        Reg_Read_Compare(ESM,REBASELINE);
        Reg_Read_Compare(CCMR4,REBASELINE);
        Reg_Read_Compare(TCMFLASH,REBASELINE);
        Reg_Read_Compare(SRAM,REBASELINE);
        Reg_Read_Compare(EFC,REBASELINE);
        Reg_Read_Compare(VIM,REBASELINE);
        Reg_Read_Compare(RTI,REBASELINE);
        Reg_Read_Compare(PBIST,REBASELINE);
        Reg_Read_Compare(STC,REBASELINE);
        retVal  = Reg_Read_Compare(PMM,COMPARE);    
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    
        Reg_Read_Compare(PMM, REBASELINE);  
        retVal = Reg_Read_Compare(PMM, COMPARE);    
    
    	retVal  = Reg_Read_Compare(CCMR4,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(EFC,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(PBIST,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(STC,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(ESM,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    
    	retVal  = Reg_Read_Compare(DCC1,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(DCC2,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(SYSTEM,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(TCMFLASH,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(SRAM,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(VIM,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    	retVal  = Reg_Read_Compare(RTI,COMPARE);
    	INCREMENT_PASS_FAIL_COUNTER(ST_PASS, retVal);
    // #endif
    /* USER CODE END */
        
        /* call the application */
    /*SAFETYMCUSW 296 S MR:8.6 <APPROVED> "Startup code(library functions at block scope)" */
    /*SAFETYMCUSW 326 S MR:8.2 <APPROVED> "Startup code(Declaration for main in library)" */
    /*SAFETYMCUSW 60 D MR:8.8 <APPROVED> "Startup code(Declaration for main in library;Only doing an extern for the same)" */
        main();
    
    /* USER CODE BEGIN (76) */
    /* USER CODE END */
    /*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */
        exit(0);
    
    /* USER CODE BEGIN (77) */
    /* USER CODE END */
    }
    
    /* USER CODE BEGIN (78) */
    /* USER CODE END */
    /** @fn void handlePLLLockFail(void)
    *   @brief This function handles PLL lock fail.
    */
    void handlePLLLockFail(void)
    {
    /* USER CODE BEGIN (79) */
    /* USER CODE END */
    	while(1)
    	{
    		
    	}
    /* USER CODE BEGIN (80) */
    /* USER CODE END */
    }
    /* USER CODE BEGIN (81) */
    /* USER CODE END */
    

    Do I need to comment out erasing of the SYS_EXCEPTION in the bootloader ?

  • Hi ,

    Apologies for the delay in late response, i was stuck with other issues.

    Do I need to comment out erasing of the SYS_EXCEPTION in the bootloader ?

    Maybe you could try this.

    Personally, i never tested _SL_Kickoff_STC_execution API with both bootloader and application.

    --
    Thanks & regards,
    Jagadish.