Part Number: MCU-PLUS-SDK-AM243X
Other Parts Discussed in Thread: TMDS243EVM
Tool/software:
Hi,
I am running am243x without os.
According to benchmark the running speed is 800MHz for the Cortex-R5F cores.
the input clock for TMDS243EVM is 25 mhz.
clock source is from TIMER8_CLOCK_SRC_MCU_HFOSC0
Am243x has 5 cores, MAIN_0_R5_0 , MAIN_0_R5_1, MAIN_1_R5_0, MAIN_1_R5_1 and m4_0
Question:
1.
So does 800Mhz means , each core speed will be 800Mhz?
Or does 800Mhz, means when all the cores run at the same time, it will be have the maximum speed of 800Mhz?
2. what would the problem if the running speed is low, is it possible msram or ddr will affect the cpu speed. But I enabled cache.
Thanks.