Part Number: AM2634
Other Parts Discussed in Thread: SYSCONFIG, UNIFLASH
Tool/software:
Hello There,
I am using AM263x- control card for my development. I want to try out the QSPI boot example.
The setup details is as follow
--
SDK - 9.2.00.55
CCs- 12.06.00.08
sysconfig - 1.20v
--
Issues
After compiling and downloading the "sbl_qspi_am263x-cc_r5fss0-0_nortos_ti-arm-clang" non-rtos example, the debugger windows shows only red stop button which is active, however the start and pause button is disable. I could not get the issue why i couldn't able to debug the example?.
When I flashed this prebuild example with uniflash i could see that QSPI example jumps to the main application after power reset. Means that, the QSPI application works from the flash then why its not working when i download the example with XDS 110xx port during debug process. is there any way to debut this example?
2nd Quetion. Is there any example available to check the bootloader sequence from the external QSPI flash.
Kindly provide support.
Thanks
Anand