Part Number: AM2632-Q1
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
We have a project in code composer for the AM2632-Q1. Attached to a SPI0 are two devices that require different clock phase. The best solution would be to configure the SPI port as multi-channel controller. I have tried that. However, Syscfg does not offer the ability to add an additional channel.
I tested this in one of the sample applications in the SDK. It works as expected.
Sysconfig is not providing a reason why this cannot be done. Are there issue that would block this ability to add multiple channels. For reference we are using the SPI controller in 3 pin mode. We are managing the CS signals to the attached devices.