This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timeout INT about UART in M3/M4

Hi,

  when progame uses fifo mode uart, how to config the receive timeout event ?  Can i change the timeout length?

  Token

 

  • The following are UART section excerpts from one of our datasheets...

    The receive timeout interrupt is asserted when the receive FIFO is not empty, and no further data is received over a 32-bit period. The receive timeout interrupt is cleared either when the FIFO becomes empty through reading all the data (or by reading the holding register), or when a 1 is written to the corresponding bit in the UARTICR register.

    All of the interrupt events are ORed together before being sent to the interrupt controller, so the UART can only generate a single interrupt request to the controller at any given time. Software can service multiple interrupt events in a single interrupt service routine by reading the UART Masked Interrupt Status (UARTMIS) register (see page 716).

    The interrupt events that can trigger a controller-level interrupt are defined in the UART Interrupt Mask (UARTIM) register (see page 709) by setting the corresponding IM bits. If interrupts are not used, the raw interrupt status is always visible via the UART Raw Interrupt Status (UARTRIS) register (see page 713).

    Interrupts are always cleared (for both the UARTMIS and UARTRIS registers) by writing a 1 to the corresponding bit in the UART Interrupt Clear (UARTICR) register (see page 719).

    ...on this particular device the timeout is not programmable and is set to a 32-bit period.

  • Joe Folkens

      Thanks,

      But The timeout is too long.

     

       Token