Part Number: AM2432
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi TI Experts,
Customer is working on AM24x, SDK: ind_comms_sdk_am243x_09_01_00_03, SysCfg: 1.18.0.
They are testing the SSC demo, they found that if they add the SPI read/write operations in the APPL_Application, when the TwinCAT reloads the slave it will cause the system reset.

Please see the modification of the code above to add the SPI inside the APPL_Application.
Another modification customer did is that they connect the TwinCAT in the SBL.
There are two situations will cause the system reset with the above code.
1: During the power on booting process, the below log shows that the system resets 4 times.

2: Reload the slave from the TwinCAT, the below log shows the system reset 1 time.

If customer does not integrate the above SPI operations code in the APPL_Application there will be no such problem.
Could you please let us know what could be the reasons for it?
Thanks,
Kevin