Tool/software:
I'm want to configure two high drive GPIOs pins for UART communication(UART0). Below are the pins which I want to convert as standard pins. Kindly share the configuration steps.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I'm want to configure two high drive GPIOs pins for UART communication(UART0). Below are the pins which I want to convert as standard pins. Kindly share the configuration steps.
Hi
The high drive GPIO only indicates these GPIO has the ability to drive high current. It is just a feature for these pins. It can not be configured in SW. You can directly treat them as a normal GPIO in the SW.
Best regards,
Cash Hao