This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SAFETI-HALCOGEN-CSP: Unit Test of FEE might be accessing data beyond the end of an array

Part Number: SAFETI-HALCOGEN-CSP
Other Parts Discussed in Thread: TMDX570LC43HDK, HALCOGEN

Tool/software:

Hello,

We are running the HALCoGen CSP Unit Tests of the FEE module on a TMDX570LC43HDK Hercules TMS570LC43x Development Kit.

We are using HALCoGen 04.07.01 and SAFETI-HALCOGEN-CSP 04.07.01.

However, I get different statement coverage results to those obtained by a colleague.
The difference is due to TI_Fee_GlobalVariables[u8EEPIndex].bWriteFirstTime.
For instance in ti_fee_writeSync.c at line 503 "if(TI_Fee_GlobalVariables[u8EEPIndex].bWriteFirstTime!=TRUE)" always evaluates to false for me. i.e. bWriteFirstTime is always TRUE

bWriteFirstTime is set to TRUE on line 242 depending upon the result from the call to TI_FeeInternal_GetCurrentBlockAddress().

The call to TI_FeeInternal_GetCurrentBlockAddress() is passed u16ArrayIndex which comes from the call to TI_FeeInternal_GetArrayIndex() on line 200.

In TI_FeeInternal_GetArrayIndex() the value of u16ArrayIndex comes from 1415 of ti_fee_util.c which is "u16ArrayIndex += Fee_BlockConfiguration[u16LoopIndex].FeeNumberOfDataSets;".
For us the number of datasets is 1.

So, in TI_Fee_WriteSync() u16ArrayIndex is 1 when it is passed to TI_FeeInternal_GetCurrentBlockAddress().
Within TI_FeeInternal_GetCurrentBlockAddress() u16ArrayIndex becomes the BlockNumber and it is used in TI_Fee_GlobalVariables[u8EEPIndex].Fee_au16BlockOffset[BlockNumber];

For us the definition of Fee_au16BlockOffset is Fee_au16BlockOffset[TI_FEE_TOTAL_BLOCKS_DATASETS]; and #define TI_FEE_TOTAL_BLOCKS_DATASETS 1U


So, in summary for us a value of 1 is used as the index into an array of only one element. i.e beyond the end of the array.

Can you confirm whether or not my understanding is correct?

I have also noticed a difference between our HALCoGen generated code and the code shown in the test results that TI provide.

In ti_fee_util.c line 1406 is "for(u16LoopIndex=0U ; u16LoopIndex<TI_FEE_NUMBER_OF_BLOCKS ; u16LoopIndex++)"
But in the test results (ti_fee_util.dyn.htm#ti_feeinternal_getarrayindex_19) the same line is
5057 (1406) for 1 0 *** 1
5058 ( 1 0 *** 1
5059 u16LoopIndex = 0U 1 0 *** 1
5060 ; 1 0 *** 1
5061 u16LoopIndex < 16U 1 0 *** 1
5062 ; 1 0 *** 1
5063 u16LoopIndex ++ 1 0 *** 1
5064 ) 1 0 *** 1

i.e. 16U instead of TI_FEE_NUMBER_OF_BLOCKS

Do you know why there is a difference?

Thank you.