Part Number: MSPM0L1227
Tool/software:
Hi,
We’ve received some inquiries from my customer. Could you answer their questions below ?
< During Flash Programming/Erasing >
During Programming/Erasing (after setting CMDEXEC register), should CPU wait for finishing Programming/Erasing ?
Or can CPU execute other processing during that ?
< DMA >
Is it possible to issue Program/Erase instruction by specifying address and data from CPU(FW) to DMA ?
Is it general way to use Flash Controller for Program/Erase ?
< Endurance of Flash (1) >
When programming only 100Byte and performing Sector Erase (1Kbyte), is the memory endurance of unprogrammed 900 bytes also counted as one time?
< Endurance of Flash (2) >
Is "Erase/program" cycle counted as one set for 100k/10k cycles of Flash memory life?
For example, if 8 bits are rewritten (1 to 0) 8 times for each 1 bit, and Erase (00h -> FFh) is performed 1 time, can the memory endurance count be counted as 1 time?
< HW Reset >
Is it no problem to leave NRST=low for a long time during VDD is supplied ?
Thanks and regards,
Hideaki