Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1105: Best pin assignment for PWM output

Part Number: MSPM0G1105
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

I am considering using MSPM0G1105 for PWM output.

The PWM will continue to output with the same period and duty from start to stop.

The PWM period is 10ms (High:9ms, Low:1ms).

Which timer is best to use? Please also advise on the key points for setting the registers inside the CPU.

Best regards,

Hiroshi Yamada