Part Number: AM2434
Tool/software:
Hi TI Experts,
Customer is working on AM24x SDK9.2, by following the below thread the functionality of ADC voltage sampling is working normal now.
However, customer found their function "bsp_AdcValueUpdata" shown below execute time is 55.4us.

It is too large for the called interrupt function frequency(8K). It is meaning that the ADC update function has occupied 44% of the entire task. Like the followed pic:

Customer may have the following two questions may need your support.
1) Why does this execution method have such a large overhead, and specifically where is the cost incurred?
2) Is there any plan to optimize this overhead and reduce the time to less than 10us?
Thanks,
Kevin