Part Number: AM2432
Tool/software:
Hi Expert,
As shown below, this is the AM243x PROC109A evm circuit diagram.
I found that the Pull-up and Pull-down resistors in Boot mode are both Pull-up,
but there is a difference between 49.9K and 10K.
Pull-down also has the same resistance value setting.
Is there any special reason?
Will there be a problem if the resistance value is not according to evm?
Thanks
Daniel