Part Number: AM2434
Tool/software:
Hi There,
About AM243-LP (AM2434) , suppose I use R5FSS0-0, 0-1, 1-0, and 1-1 (i.e. use all 4 R5F cores). I understand the allocation is as follows.
core 0-0: 32KB TCMA, 16 KB TCMB0, 16 KB TCMB1
core 0-1: 32KB TCMA, 16 KB TCMB0, 16 KB TCMB1
core 1-0: 32KB TCMA, 16 KB TCMB0, 16 KB TCMB1
core 1-1: 32KB TCMA, 16 KB TCMB0, 16 KB TCMB1
Is the aforementioned allocation correct? Is it possible to have a piece of TCM (either TCMA or TCMB or both) visible to both core 0-0 and core 0-1?
Best regards,
Jinlong