Part Number: LP-MSPM0G3507
Tool/software:
Hey.
I am trying to understand the cross triggering, but I'm probably a bit daft, since I cant quite understand the datasheet and reference manual on the matter.
I have tried to set up two timers, where I want the up-counting compare event to cross trigger the second timer.
I know that two of the timers have a phase-shift capability, but I wonder if it would be possible to synchronize in this fasion?
The reason is, that I have a project where I need to generate four synchronized pwm's with the same period, but different (controllable) phase.
I have tried to set up a cross-trigger synchronization between TIMA0 and TIMA1, but I can' manage to get it to work.
I hope someone would give a "dumbed-down" walkthrough of how I would do this.
Regards
Anders