This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: MQTT DATA RATE : I am not able to send more than 980 bytes of payload of data to the mosquitto broker. WHAT IS THE MAX PAYLOAD LIMIT WITHOUT LOSS FOR THIS HARDWARE??

Part Number: MSP432E401Y

Tool/software:

I tried to send a payload of more than 980 bytes of data through a the dev board . I connected it to a CE510 PHAROS Router and have a laptop running a mosquitto broker connected to one more CE router. But the data gets lost if the payload is more than 980 bytes. Is there a way to increase the the payload size without data loss . What is the issue?? I AM USING TI RTOS CODE FOR THIS ..