Part Number: TMS570LC4357-EP
Tool/software:
Hello,
We have ported the CoreMark benchmark software (https://www.eembc.org/coremark/) to run on the TMS570LC43 EVM board (using CCS and "TI v20.2.7.LTS" compiler toolchain). The results we have observed, are:
CoreMark 1.0 score on TMS570LC43:
---
No optimization: 45.55
Level 0 optimization: 103.11
Level 1 optimization: 113.90
Level 2 optimization: 148.35
Level 3 optimization: 152.89
Level 4 optimization: 155.63
Our TMS570LC43 EVM CPU clock (GCLK) config when running the CoreMark code, is:

Hence, the CPU should be running at 200MHz, if we are not mistaken.
We would like to inquire about whether the observed CoreMark results are expected, on TMS570LC43? Please advise.
Thank you.
John