Part Number: AM263P4
Other Parts Discussed in Thread: TMDSCNCD263P, SYSCONFIG
Tool/software:
Hi,
My customer wants to connect two memory devices on OSPI interface, like AM263Px Control Card (TMDSCNCD263P).
Below is Control Card connection. NOR and NAND are connected.
The customer wants to connect two NORs (IS25LX256).
But Sysconfig generates an error saying "Same device cannot be selected". Does it mean same two NORs cannot be connected?
And Sysconfig detects some signals (data) are conflicted and generates an error "Maximum of 1 instance allowed."
Questions:
Q1) Is it OK to connect two memory devices on OSPI interface using CS0/CS1 as same as TMDSCNCD263P?
(I thought connecting two devices are not supported on other devices, such as AM243x, AM64x.)
Q2) If the answer to Q1) is yes, could you tell me how to configure sysconfig?
Thanks and regards,
Koichiro Tashiro