Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I have a project that requires both internal op-amps (OPA_0 and OPA_1) and the positive input of both OPA should be connected to the same voltage reference.
From the code composer Sysconfig tool, I am not able to select the same GPIO for both positive inputs (PA25).
I got the following error on OPA_1 config : "PA25/29 is currently in use by OPA 0 and is also only available on OPA0 which is in use by OPA 0".
Is this a limitation of the Sysconfig tool ?
Is there a way to use the same pin on both amplifiers in order to keep 1 pin for another usage ?
MCU reference : MSPM0L1306TRGER
Regards
Alexandre.