Part Number: AM2632
Tool/software:
Hi,
can customer add an extended OID to the x509 certificate from SBL and the application?
For their end customer they need additional information for verification and integration into the CA which would be the cleanest solution.The value is a 32-bit integer.
Since they also provide the extension for the SBL, the FBL (ROM bootloader) would also have to cope with this OID resp. he can just ignore it.
Is that possible?
Regards, Holger