This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2612: Code running in TCMA is slower than OCRAM

Part Number: AM2612

Tool/software:

To test the runtime of the modified iqmath function, I executed it in both TCMA and OCRAM. 

My environment is CCS12.8,SDK 10.0.0.37   code optimization O-fast

To prevent caching of identical computation results, to prevent caching of identical computation results, I generated 100 random numbers for calculation. Modify USE_TCM to 0 or 1 to choose whether to allocate memory to TCM. Here is my test code:

#include <stdlib.h>
#include <math.h>
#include <kernel/dpl/DebugP.h>
#include "ti_drivers_config.h"
#include "ti_board_config.h"
#include "IQmathLib.h"

#include "mathlib/trig/ti_arm_trig.h"

uint32_t u32TimerStart,u32TimerLoad = 0;
float f32DataOut;
_iq iqDataOut;

float f32SinOut_assembly[100] = {0.0f};
_iq iqSinOut_assembly[100] = {0};
_iq iqSinOut[100] = {0};

float f32SqrtOut_assembly[100] = {0.0f};
_iq iqSqrtOut[100] = {0};
_iq iqSqrtOut_assembly[100] = {0};
_iq iqMulOut[100] = {0};
_iq iqMulOut_assembly[100] = {0};
_iq iqDivOut[100] = {0};
_iq iqDivOut_assebmly[100] = {0};
#define USE_TCM (0)

const float iq2fScale = 0.000000059604645f;
const float f2iqScale = 16777216.000000f;
const float pi2 = 6.28318530717959f;
float f32SinIn[100] = {3.712407,2.129162,5.611364,2.936816,4.674741,2.058908,4.290381,3.632543,3.796699,3.349105,
                        5.616087,5.240428,4.939541,3.788255,4.763273,2.698073,4.023251,1.531706,1.085435,0.777734,
                        3.323697,3.257371,3.88798,0.794623,5.438464,4.107997,2.541916,0.399682,5.709745,2.603319,
                        1.950818,2.565326,4.598627,5.130248,4.920356,4.647836,4.717129,2.899751,5.836289,2.917093,
                        4.305292,0.280102,4.348784,1.12106,5.377209,4.169042,4.815597,4.29549,1.702546,2.472285,
                        6.189092,4.855415,0.300805,1.388049,1.028099,1.881404,2.062716,5.260398,3.941642,4.493471,
                        6.282049,6.160821,5.930238,1.333015,1.343667,6.184921,4.436584,5.315681,5.676171,5.921862,
                        3.521913,3.320549,1.552201,2.712443,0.376286,3.635715,1.884349,0.299,2.111523,3.769371,
                        5.138324,0.649593,0.209134,5.092558,4.008929,4.508341,2.642054,3.749132,5.33098,1.087774,
                        0.691124,6.164273,2.357287,5.472303,2.197861,5.667922,3.463029,2.620582,2.690765,4.312372};

float f32SqrtIn[100] = {0.822207,0.966454,0.090616,0.788111,0.758306, 0.738356,0.535171,0.015758,0.042506,0.825861,
                        0.971483,0.975205,0.510375,0.36407,0.889855,0.646937,0.759267,0.143709,0.237777,0.557448,
                        0.593504,0.926576,0.204938,0.673273,0.98163,0.171916,0.745332,0.17287,0.131861,0.928158,
                        0.968507,0.998606,0.004652,0.270313,0.162947,0.251017,0.281967,0.416146,0.870192,0.406895,
                        0.554871,0.084685,0.169093,0.274182,0.897739,0.353732,0.468215,0.730876,0.421698,0.258417,
                        0.742467,0.138787,0.878365,0.837744,0.045111,0.926592,0.147535,0.312763,0.556087,0.552088,
                        0.698499,0.479554,0.66014,0.352169,0.720769,0.136011,0.925598,0.243663,0.08588,0.900161,
                        0.820419,0.191058,0.715925,0.431502,0.662533,0.294721,0.263202,0.331849,0.017807,0.782637,
                        0.449799,0.44025,0.351247,0.129914,0.490479,0.057155,0.673106,0.735046,0.91323,0.811223,
                        0.51295,0.657512,0.328113,0.386043,0.23684,0.636593,0.336395,0.463664,0.865202,0.683065};

_iq iqSinIn[100] = {7334100,14626481,5558979,16234385,8725661,14385339,766440,12523141,7860266,15542651,
                    3058682,3530925,835795,5314808,14040525,7786403,10551614,15150083,10332709,14607518,
                    5518319,3604083,6894421,13978931,15174124,10682735,1219195,10832689,5532140,14037653,
                    4911997,3658046,868993,14653156,10694315,12878234,13577655,15698950,2119409,2332973,
                    7977791,14565738,14066455,14586520,6719596,14170681,15345733,7350,7163648,16170356,
                     7602036,12090923,58194,15940078,16617123,14004457,9826022,5269094,13714629,11069671,
                     15910489,9096013,4339855,3857399,12516740,16637451,15557704,7368087,11601717,6268786,
                     2355206,7485576,10352497,8882846,1878697,10673338,11435463,15731345,10656716,1784939,
                     10150870,12403372,14052832,8038175,14558343,7754627,6368348,8329271,5593392,37961,
                     643991,3092709,9125990,8477608,4168482,1193493,849605,10194797,10043572,807661};

_iq iqSqrtIn[100] = {7334100,14626481,3558979,16234385,8725661,14385339,766440,12523141,7860266,15542651,
                     3058682,3530925,835795,5314808,14040525,7786403,10551614,15150083,10332709,14607518,
                     5518319,3604083,6894421,13978931,15174124,10682735,1219195,10832689,5532140,14037653,
                     4911997,3658046,868993,14653156,10694315,12878234,13577655,15698950,2119409,2332973,
                     7977791,14565738,14066455,14586520,6719596,14170681,15345733,7350,7163648,16170356,
                     7602036,12090923,58194,15940078,16617123,14004457,9826022,5269094,13714629,11069671,
                     15910489,9096013,4339855,3857399,12516740,16637451,15557704,7368087,11601717,6268786,
                     2355206,7485576,10352497,8882846,1878697,10673338,11435463,15731345,10656716,1784939,
                     10150870,12403372,14052832,8038175,14558343,7754627,6368348,8329271,5593392,37961,
                     643991,3092709,9125990,8477608,4168482,1193493,849605,10194797,10043572,807661};

_iq iqDivIn[100] =  {16316244,15787933,15403241,11660262,4292734,9032192,10156213,7448221,10866686,14014676,
                     2452939,14082717,12075177,9806672,7991054,15986104,13088964,8940713,10375408,1346096,
                     8174168,8122380,974020,3198849,4218291,13775288,11396425,1263821,1258931,7047291,
                     13876626,5835055,6033813,9030130,4699562,11870098,14387270,8957787,4657818,1399007,
                     357767,438226,6696376,3528846,11882848,6023232,5521753,16317692,7982752,8484968,
                     665438,2786828,8893826,409544,110629,11880945,16759713,8739897,16023258,5975345,
                     5728985,10647452,11059773,10276916,15088830,10948835,4058958,3323378,6170826,16629831,
                     10360173,10079387,1982317,7093657,7846383,2783815,2542736,12446418,14328632,12115202,
                     1384528,11408496,907709,2625221,640234,1981499,15247266,13513537,1234216,13163128,
                     3786184,4005491,8754898,10964149,1142647,8962164,4370648,10053798,15926282,10122239
};

#if USE_TCM
__attribute__((__section__(".armiqmath"), noinline))_iq24 _IQ24mpy_test(_iq A, _iq B)
#else
static __attribute__((__section__(".armiqmath")))_iq24 _IQ24mpy_test(_iq A, _iq B)
#endif
{
    _iq24 result;
    __asm__ volatile(
        "smull   r2, r3, %1, %2       \n" // r2 = lower 32bit r3 = higher 32bit
        "lsr     r2, r2, #24          \n" // r2 >> 24
        "orr     r2, r2, r3, lsl #8   \n" // combine r3's 8bit high with r2's 8bit low
        "mov     %0, r2               \n" // save result
        : "=r" (result)
        : "r" (A), "r" (B)
        : "r2", "r3", "cc"
    );
    return result;
}
#if USE_TCM
__attribute__((__section__(".armiqmath"), noinline))_iq24  _IQdiv_test(_iq iqDividend, _iq iqDivisor)
#else
static __attribute__((__section__(".armiqmath")))_iq24  _IQdiv_test(_iq iqDividend, _iq iqDivisor)
#endif
{
    _iq24 result;
    __asm__ volatile (
        "cmp    %2, #0                \n" // if iqDivisor == 0
        "beq    1f                    \n" // jump to 1
        "vmov    s0, %1               \n" // s0 =  iqDividend
        "vmov    s1, %2               \n" // s1 =  iqDivisor
        "vcvt.f32.s32   s0, s0        \n" // iqDividend to float-point
        "vcvt.f32.s32   s1, s1        \n" // iqDivisor to float-point
        "vdiv.f32       s2, s0, s1    \n" // s2 = s0/s1
        "vmov.f32       s3, %3        \n" // s3 = f2iqScale
        "vmul.f32       s2, s2, s3    \n" // f2iqScale fix-point
        "vcvt.s32.f32   s2, s2        \n" // result to fix-point
        "vmov           %0, s2        \n" // save result
        "b      2f                    \n" // skip 1
        "1:                           \n"
        "mov    %0, #0                \n" // if divisor = 0, return 0
        "2:                           \n"
        : "=r" (result)                // output result
        : "r" (iqDividend), "r" (iqDivisor), "r" (f2iqScale)
        : "s0", "s1", "s2", "s3", "cc", "memory"
    );
    return result;
}

#if USE_TCM
__attribute__((__section__(".armiqmath"), noinline))_iq24 _IQ24sin_test1(const _iq inputIq24Num)
#else
static __attribute__((__section__(".armiqmath")))_iq24 _IQ24sin_test1(const _iq inputIq24Num)
#endif
{
    _iq iqSinResult;
    float floatSinResult;
    float inputFloatNum;

    __asm__ volatile (
        "vmov    s0, %1               \n" // s0 = inputIq24Num
        "vcvt.f32.s32 s0, s0          \n" // fix-point to float-point
        "vmov.f32 s1, %2              \n" // s1 = iq2fScale
        "vmul.f32 s0, s0, s1          \n" // s0 = s0*s1
        "vmov.f32 s2, %3              \n" // s2 = 2pi
        "vmul.f32 s0, s0, s2          \n" // s0 = s0*2pi, so input is range in (0,2pi)
        "vmov    %0, s0               \n" // save s0 to inputFloatNum
        : "=r" (inputFloatNum)
        : "r" (inputIq24Num), "r" (iq2fScale), "r" (pi2)
        : "s0", "s1", "s2", "cc", "memory"
    );
    floatSinResult = ti_arm_sin(inputFloatNum); // call ti_arm_sin

    __asm__ volatile (
        "vmov    s0, %1               \n" // s0 = floatSinResult
        "vldr    s1, [%2]             \n" // s1 = f2iqScale
        "vmul.f32 s0, s0, s1          \n" // s0 = s0*s1
        "vcvt.s32.f32 s0, s0          \n" // float-point to fix-point
        "vmov    %0, s0               \n" // save result
        : "=r" (iqSinResult)
        : "r" (floatSinResult), "r" (&f2iqScale)
        : "s0", "s1", "cc", "memory"
    );

    return iqSinResult;
}


#if USE_TCM
__attribute__((__section__(".armiqmath"), noinline))_iq24 _IQ24sqrt_test1(const _iq inputIq24Num)
#else
static __attribute__((__section__(".armiqmath")))_iq24 _IQ24sqrt_test1(const _iq inputIq24Num)
#endif
{
    _iq24 iqSinResult;
    float floatSinResult;
    float inputFloatNum;
    __asm__ volatile (
        "vmov    s0, %1           \n"
        "vcvt.f32.s32 s0, s0      \n"
        "vmov.f32 s1, %2          \n"
        "vmul.f32 s0, s0, s1      \n"
        "vmov    %0, s0           \n"
        : "=r" (inputFloatNum)
        : "r" (inputIq24Num), "r" (iq2fScale)
        : "s0", "s1", "cc", "memory"
    );
    floatSinResult = ti_arm_sqrt(inputFloatNum);
    __asm__ volatile (
        "vmov    s0, %1               \n"
        "vldr    s1, [%2]             \n"
        "vmul.f32   s0, s0, s1        \n"
        "vcvt.s32.f32 s0, s0          \n"
        "vmov    %0, s0               \n"
        : "=r" (iqSinResult)
        : "r" (floatSinResult), "r" (&f2iqScale)
        : "s0", "s1", "cc", "memory"
    );
    return iqSinResult;
}


int mathLib_test_main(void)
{
    System_init();
    Board_init();

#if USE_TCM
    DebugP_log("USE TCM\r\n");
#else
    DebugP_log("NOT USE TCM\r\n");
#endif

    DebugP_log("sine test\r\n");

    //sin

    u32TimerStart = ReadCpuTimer0Counter();
    for(int i = 0;i<100;i++)
    {
        iqSinOut_assembly[i] = _IQ24sin_test1(iqSinIn[i]);
    }
    u32TimerLoad = ReadCpuTimer0Counter() - u32TimerStart;
    DebugP_log("assembly IQsin:%d\r\n",u32TimerLoad);

    DebugP_log("sqrt test\r\n");

    //sqrt

    u32TimerStart = ReadCpuTimer0Counter();
    for(int i = 0;i<100;i++)
    {
        iqSqrtOut_assembly[i] = _IQ24sqrt_test1(iqSqrtIn[i]);
    }
    u32TimerLoad = ReadCpuTimer0Counter() - u32TimerStart;
    DebugP_log("assembly sqrt:%d\r\n",u32TimerLoad);

    DebugP_log("mult test\r\n");

    //mul

    u32TimerStart = ReadCpuTimer0Counter();
    for(int i = 0;i<100;i++)
    {
        iqMulOut_assembly[i] = _IQ24mpy_test(iqSinIn[i], iqSqrtIn[i]);
    }
    u32TimerLoad = ReadCpuTimer0Counter() - u32TimerStart;
    DebugP_log("assembly mpy:%d\r\n",u32TimerLoad);


    DebugP_log("div test\r\n");

    //div

    u32TimerStart = ReadCpuTimer0Counter();
    for(int i = 0;i<100;i++)
    {
        iqDivOut_assebmly[i] = _IQdiv_test(iqDivIn[i], iqSqrtIn[i]);
    }
    u32TimerLoad = ReadCpuTimer0Counter() - u32TimerStart;
    DebugP_log("assebmly iq div:%d\r\n",u32TimerLoad);
    while(1)
    {};
}

besides, need to configure RTI to represent time, I configured RTI to 125count = 1us

uint32_t ReadCpuTimer0Counter(void)
{
    uint32_t u32Timer = 0xFFFFFFFF - HW_RD_REG32(RTI_CPU_BASE_ADDR + CSL_RTI_RTIFRC0);
    return u32Timer;
}

my cmd file:


 /* This is the stack that is used by code running within main()
  * In case of NORTOS,
  * - This means all the code outside of ISR uses this stack
  * In case of FreeRTOS
  * - This means all the code until vTaskStartScheduler() is called in main()
  *   uses this stack.
  * - After vTaskStartScheduler() each task created in FreeRTOS has its own stack
  */

 --stack_size=16384
/* This is the heap size for malloc() API in NORTOS and FreeRTOS
* This is also the heap used by pvPortMalloc in FreeRTOS
*/
 --heap_size=32768
-e_vectors  /* This is the entry of the application, _vector MUST be placed starting address 0x0 */

/* This is the size of stack when R5 is in IRQ mode
 * In NORTOS,
 * - Here interrupt nesting is enabled
 * - This is the stack used by ISRs registered as type IRQ
 * In FreeRTOS,
 * - Here interrupt nesting is enabled
 * - This is stack that is used initally when a IRQ is received
 * - But then the mode is switched to SVC mode and SVC stack is used for all user ISR callbacks
 * - Hence in FreeRTOS, IRQ stack size is less and SVC stack size is more
 */
__IRQ_STACK_SIZE = 256;
/* This is the size of stack when R5 is in IRQ mode
 * - In both NORTOS and FreeRTOS nesting is disabled for FIQ
 */
__FIQ_STACK_SIZE = 256;
__SVC_STACK_SIZE = 4096; /* This is the size of stack when R5 is in SVC mode */
__ABORT_STACK_SIZE = 256;  /* This is the size of stack when R5 is in ABORT mode */
__UNDEFINED_STACK_SIZE = 256;  /* This is the size of stack when R5 is in UNDEF mode */



SECTIONS
{
    .vectors  : {    } > R5F_VECS   , palign(8)


    GROUP  :   {
	    .text.hwi : {    } palign(8)
	    .text.cache : {    } palign(8)
	    .text.mpu : {    } palign(8)
	    .text.boot : {    } palign(8)
	    .text:abort : {    } palign(8)
    } > OCRAM


    GROUP  :   {
	    .text : {    } palign(8)
	    .rodata : {    } palign(8)
    } > OCRAM


    GROUP  :   {
    .data : {    } palign(8)
    } > OCRAM


    GROUP  :   {
	    .bss : {    } palign(8)
	    RUN_START(__BSS_START)
	    RUN_END(__BSS_END)
	    .sysmem : {    } palign(8)
	    .stack : {    } palign(8)
	    .usbCxtRam : {    } align(8)
    } > OCRAM


    GROUP  :   {
	    .irqstack : {        . = . + __IRQ_STACK_SIZE;    } align(8)
	    RUN_START(__IRQ_STACK_START)
	    RUN_END(__IRQ_STACK_END)
	    .fiqstack : {        . = . + __FIQ_STACK_SIZE;    } align(8)
	    RUN_START(__FIQ_STACK_START)
	    RUN_END(__FIQ_STACK_END)
	    .svcstack : {        . = . + __SVC_STACK_SIZE;    } align(8)
	    RUN_START(__SVC_STACK_START)
	    RUN_END(__SVC_STACK_END)
	    .abortstack : {        . = . + __ABORT_STACK_SIZE;    } align(8)
	    RUN_START(__ABORT_STACK_START)
	    RUN_END(__ABORT_STACK_END)
	    .undefinedstack : {        . = . + __UNDEFINED_STACK_SIZE;    } align(8)
	    RUN_START(__UNDEFINED_STACK_START)
	    RUN_END(__UNDEFINED_STACK_END)
    } > OCRAM


    GROUP  :   {
    .ARM.exidx : {    } palign(8)
    .init_array : {    } palign(8)
    .fini_array : {    } palign(8)
    } > OCRAM

    .bss.user_shared_mem (NOLOAD) : {    } > USER_SHM_MEM

    .bss.log_shared_mem (NOLOAD) : {    } > LOG_SHM_MEM

    .bss.ipc_vring_mem (NOLOAD) : {    } > RTOS_NORTOS_IPC_SHM_MEM

    .bss.sipc_hsm_queue_mem (NOLOAD) : {    } > MAILBOX_HSM

    .bss.sipc_secure_host_queue_mem (NOLOAD) : {    } > MAILBOX_R5F


    GROUP  :   {
    	.bss.nocache : {    } align(8)
    } > NON_CACHE_MEM

    armiqmath  : {    } > R5F_TCMA   , palign(8)


}


MEMORY
{
    R5F_VECS   : ORIGIN = 0x0 , LENGTH = 0x40
    R5F_TCMA   : ORIGIN = 0x40 , LENGTH = 0x7FC0
    R5F_TCMB   : ORIGIN = 0x80000 , LENGTH = 0x8000
    SBL   : ORIGIN = 0x70000000 , LENGTH = 0x40000
    OCRAM   : ORIGIN = 0x70040000 , LENGTH = 0xC0000
    NON_CACHE_MEM   : ORIGIN = 0x70100000 , LENGTH = 0x8000
    USER_SHM_MEM   : ORIGIN = 0x70150000 , LENGTH = 0x4000
    LOG_SHM_MEM   : ORIGIN = 0x70154000 , LENGTH = 0x4000
    FLASH   : ORIGIN = 0x60100000 , LENGTH = 0x80000
    RTOS_NORTOS_IPC_SHM_MEM   : ORIGIN = 0x72000000 , LENGTH = 0x3E80
    MAILBOX_HSM   : ORIGIN = 0x44000000 , LENGTH = 0x3CE
    MAILBOX_R5F   : ORIGIN = 0x44000400 , LENGTH = 0x3CE

    /* For memory Regions not defined in this core but shared by other cores with the current core */


}

The results of running the code with and without TCM are as follows:

[Cortex_R5_0] NOT USE TCM
sine test
assembly IQsin:-2026
sqrt test
assembly sqrt:-1075
mult test
assembly mpy:-331
div test
assebmly iq div:-995

[Cortex_R5_0] USE TCM
sine test
assembly IQsin:-2195
sqrt test
assembly sqrt:-1420
mult test
assembly mpy:-630
div test
assebmly iq div:-1270

The results showed that the function ran faster in OCRAM; why is this?

I have uploaded the iqmathLib. h file that needs to be included in the code in the attachment

IQmathLib.h

  • Hi Zhou,

    Apologies for delayed response allow me sometime to check this on my end and get back to you by next week Wednesday 

  • Ok understood the issue Zhou. I am working on it. 

  • Hi Zhou,

    Referring to the following link from ARM documetation: Performance of TCM compared to cache

    In certain situations, TCM performance is better than cache performance. In other situations, cache performance is better than TCM performance.

    If an instruction or data fetch misses in the cache, the processor fetches from the external memory. In this case the performance of the TCM is significantly better than the cache. This is because the cache miss requires an external memory fetch and allocation of data into the cache.

    However, if the instructions and data have been pre-fetched from external memory, populating the processor caches, then for subsequent fetches of the cached instructions and data, the cache performance compared to TCM performance is different:

    • For data fetches, TCM performance will generally be comparable to cache performance, when there is a cache hit.

    • For instruction fetches, TCM performance is a little lower than cache performance.

    Let me know if this helps!

    Regards,
    Akshit

  • Hi Akshit,

         I understand now, so in cases where mathematical libraries are placed in TCM and involve variables being read from the external memory, it may not necessarily be suitable for TCM. Perhaps TCM is better suited for functions with fixed execution steps.

  • Hi Zhou

    Yes, your understanding seems correct. Tightly Coupled Memory (TCM) is designed for high-speed access and is typically used for critical code paths or functions that require predictable execution times.

    1. Fixed Execution Steps: TCM is well-suited for functions with fixed execution steps, such as real-time control algorithms, where timing and performance are critical.

    2. Avoiding External Memory Access: If a function relies heavily on variables stored in external memory, it may not benefit from the speed advantages of TCM. Accessing external memory can introduce latency that negates the performance benefits of using TCM. 

    3. Mathematical Libraries: If mathematical libraries involve dynamic memory allocation or frequent access to external variables, they may not be suitable for TCM. Instead, functions that can operate on fixed data or that have predictable memory access patterns are better candidates for TCM.

    4. TCM is ideal for interrupt service routines (ISRs), state machines, and other time-sensitive operations where execution speed is important.

    For more detailed information, you can refer to the Technical Reference Manual (TRM), which provides insights into the architecture and best practices for using TCM effectively.