Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hey. Im trying to set up TIMA0 to cross-trigger TIMA1 for one-shots, but I must be misunderstanding something....
When TIMA1 is set up to repeat (
If I use different LOAD values (TIMA0=1000, TIMA1=300), I can see that TIMA1 has a reload when TIMA0 has a compare-up event.
But if I set TIMA1 to not repeat - for one-shots - then it does not trigger at all.
This does generate a one-shot on TIMA1.
So I wonder:
Why does TIMA0 generate a trigger on every compare-up events if TIMA1 is set to REPEAT=1, but not if TIMA1 is set to REPEAT=0??
What am I missing?
Here's the code:
#include <ti/driverlib/m0p/dl_interrupt.h>
#include "ti_msp_dl_config.h"
void setup();
int main(void)
{
setup();
while (1)
{
}
}
void setup()
{
SYSCFG_DL_initPower(); // Reset & Enable power to peripherals
// Set up the pin mux. PINCM19 = PA8, PINCM39 = PA17
IOMUX->SECCFG.PINCM[IOMUX_PINCM19] = (IOMUX_PINCM19_PF_TIMA0_CCP0 | IOMUX_PINCM_PC_CONNECTED);
IOMUX->SECCFG.PINCM[IOMUX_PINCM39] = (IOMUX_PINCM39_PF_TIMA1_CCP0 | IOMUX_PINCM_PC_CONNECTED);
GPIOA->DOESET31_0 = (DL_GPIO_PIN_8 | DL_GPIO_PIN_17);
SYSCFG_DL_SYSCTL_init(); // Enable clocks, and some system thingimabobs.
///////////////////////////////////// PWM setup //////////////////////////////////////
// 1 - Clocking
TIMA0->CLKSEL = GPTIMER_CLKSEL_BUSCLK_SEL_ENABLE;
TIMA0->CLKDIV = GPTIMER_CLKDIV_RATIO_DIV_BY_8;
TIMA0->COMMONREGS.CPS = 39U;
TIMA1->CLKSEL = GPTIMER_CLKSEL_BUSCLK_SEL_ENABLE;
TIMA1->CLKDIV = GPTIMER_CLKDIV_RATIO_DIV_BY_8;
TIMA1->COMMONREGS.CPS = 39U;
// 2 - CCACT CC pin actions: High on zero, low on compare-up
uint32_t CCACT_MASK = (GPTIMER_CCACT_01_SWFRCACT_CMPL_MASK | GPTIMER_CCACT_01_SWFRCACT_MASK |
GPTIMER_CCACT_01_FEXACT_MASK | GPTIMER_CCACT_01_FENACT_MASK |
GPTIMER_CCACT_01_CC2UACT_MASK | GPTIMER_CCACT_01_CC2DACT_MASK |
GPTIMER_CCACT_01_CUACT_MASK | GPTIMER_CCACT_01_CDACT_MASK |
GPTIMER_CCACT_01_LACT_MASK | GPTIMER_CCACT_01_ZACT_MASK);
uint32_t actions = (GPTIMER_CCACT_01_ZACT_CCP_HIGH | GPTIMER_CCACT_01_CUACT_CCP_LOW);
TIMA0->COUNTERREGS.CCACT_01[0] = (TIMA0->COUNTERREGS.CCACT_01[0] & ~CCACT_MASK) | (actions & CCACT_MASK);
TIMA1->COUNTERREGS.CCACT_01[0] = (TIMA1->COUNTERREGS.CCACT_01[0] & ~CCACT_MASK) | (actions & CCACT_MASK);
// 3 - CCCTL Compare mode, Load COND on CCP trigger rise, updates to CC written immediately.
uint32_t CCCTL_MASK = (GPTIMER_CCCTL_01_COC_MASK | GPTIMER_CCCTL_01_ZCOND_MASK |
GPTIMER_CCCTL_01_LCOND_MASK | GPTIMER_CCCTL_01_ACOND_MASK |
GPTIMER_CCCTL_01_CCOND_MASK);
uint32_t mode_Conds = (GPTIMER_CCCTL_01_COC_COMPARE | GPTIMER_CCCTL_01_CCUPD_IMMEDIATELY);
TIMA0->COUNTERREGS.CCCTL_01[0] = (TIMA0->COUNTERREGS.CCCTL_01[0] & ~CCCTL_MASK) | (mode_Conds & CCCTL_MASK);
mode_Conds |= GPTIMER_CCCTL_01_LCOND_CC_TRIG_RISE;
TIMA1->COUNTERREGS.CCCTL_01[0] = (TIMA1->COUNTERREGS.CCCTL_01[0] & ~CCCTL_MASK) | (mode_Conds & CCCTL_MASK);
// 4 - OCTL CCP Initally low, no invertion, use generator out.
TIMA0->COUNTERREGS.OCTL_01[0] = (GPTIMER_OCTL_01_CCPIV_LOW | GPTIMER_OCTL_01_CCPOINV_NOINV | GPTIMER_OCTL_01_CCPO_FUNCVAL);
TIMA1->COUNTERREGS.OCTL_01[0] = (GPTIMER_OCTL_01_CCPIV_LOW | GPTIMER_OCTL_01_CCPOINV_NOINV | GPTIMER_OCTL_01_CCPO_FUNCVAL);
// 5 - IFCTL No invert, use trigger input
uint32_t IFCTL_MASK = (GPTIMER_IFCTL_01_INV_MASK | GPTIMER_IFCTL_01_ISEL_MASK);
uint32_t input = (GPTIMER_IFCTL_01_INV_NOINVERT | GPTIMER_IFCTL_01_ISEL_TRIG_INPUT);
TIMA1->COUNTERREGS.IFCTL_01[0] = (TIMA1->COUNTERREGS.IFCTL_01[0] & ~IFCTL_MASK) | (input & IFCTL_MASK);
// 6 - LOAD pwm period = 1000
TIMA0->COUNTERREGS.LOAD = 1000;
TIMA1->COUNTERREGS.LOAD = 300;
// 7 - CTRCTL CVAE=0,
uint32_t CTRCTL_MASK = (GPTIMER_CTRCTL_CZC_MASK | GPTIMER_CTRCTL_CAC_MASK |
GPTIMER_CTRCTL_CLC_MASK | GPTIMER_CTRCTL_CVAE_MASK |
GPTIMER_CTRCTL_CM_MASK | GPTIMER_CTRCTL_REPEAT_MASK |
GPTIMER_CTRCTL_EN_MASK);
uint32_t ctrctl_val = (GPTIMER_CTRCTL_REPEAT_REPEAT_1 | GPTIMER_CTRCTL_CM_UP | GPTIMER_CTRCTL_EN_DISABLED | GPTIMER_CTRCTL_CVAE_ZEROVAL);
TIMA0->COUNTERREGS.CTRCTL = (TIMA0->COUNTERREGS.CTRCTL & ~CTRCTL_MASK) | (CTRCTL_MASK & ctrctl_val);
ctrctl_val = (GPTIMER_CTRCTL_REPEAT_REPEAT_1 | GPTIMER_CTRCTL_CM_UP | GPTIMER_CTRCTL_EN_DISABLED | GPTIMER_CTRCTL_CVAE_ZEROVAL);
TIMA1->COUNTERREGS.CTRCTL = (TIMA1->COUNTERREGS.CTRCTL & ~CTRCTL_MASK) | (CTRCTL_MASK & ctrctl_val);
// 8 - DUTY CYCLE (compare value)
TIMA0->COUNTERREGS.CC_01[0] = 610;
TIMA1->COUNTERREGS.CC_01[0] = 229;
// 9 - ENABLE CLOCK
TIMA0->COMMONREGS.CCLKCTL = GPTIMER_CCLKCTL_CLKEN_ENABLED;
TIMA1->COMMONREGS.CCLKCTL = GPTIMER_CCLKCTL_CLKEN_ENABLED;
// 10 - SET CCP DIRECTION
TIMA0->COMMONREGS.CCPD = GPTIMER_CCPD_C0CCP0_OUTPUT;
TIMA1->COMMONREGS.CCPD = GPTIMER_CCPD_C0CCP0_OUTPUT;
// 11 - TRIGGER CONTROL
TIMA0->COMMONREGS.CTTRIGCTL = (GPTIMER_CTTRIGCTL_EVTCTTRIGSEL_CCU0 | GPTIMER_CTTRIGCTL_EVTCTEN_ENABLE | GPTIMER_CTTRIGCTL_CTEN_ENABLE);
// 12 - TSEL Trigger select
TIMA1->COUNTERREGS.TSEL = (TIMA1->COUNTERREGS.TSEL & ~GPTIMER_TSEL_ETSEL_MASK) | (GPTIMER_TSEL_ETSEL_TRIG0 & GPTIMER_TSEL_ETSEL_MASK);
TIMA1->COUNTERREGS.TSEL |= (GPTIMER_TSEL_TE_ENABLED);
TIMA0->COUNTERREGS.CTRCTL |= GPTIMER_CTRCTL_EN_ENABLED; // Start the main timer
//TIMA0->COMMONREGS.CTTRIG = GPTIMER_CTTRIG_TRIG_GENERATE; // Manually generate trigger
}