Part Number: MSPM0G1105
Tool/software:
I am considering configuring a BSL using I2C.
What is the relationship between the master and slave?
Master: Host (PC, etc.) side
Slave: CPU side (MSPM0G1105)
Is it the right one?
The SLAU887 documentation states that the default I2C target address is 0x48, so I think the CPU side is the slave.
One more question:
If I only need to rewrite the program from the host, it should be fine to connect only SCL and SDA, right?
Please let me know.
Hiroshi Yamada