Part Number: MSPM0G1507
Other Parts Discussed in Thread: UNIFLASH, , MSPM0G3507, SYSCONFIG
Tool/software:
Hallo,
I`ve been using CCS Theia 1.5.1 for a while now without any issues. Last week I installed CCS 20 and imported my Theia 1.5.1 project without any issues.
After I`ve started my first debugging session with CCS 20 (flash download was complete), I couldn`t start any debug sessions anymore. I´ve got the error "The target indicates there is an error condition from a previous SWD request".
Until then I´ve been debugging the same device for at least 1000 times. Same setup -> XDS110. The issue above happend after I installed CCS20.
I`m writing to NONMAIN because I want to disable the BSL because I´m using PA18 for other purposes. I`ve checked Erase MAIN and NONMAIN in the debug session config.
Since then I`ve tried the following:
1. Factory Reset via Script in CCS 20 -> as mentioned in many other threads -> same error
2. Factory reset via Online Tool
3. Factory reset via Uniflash 8.8.1 -> same error
4. Changed the Chip on the board (desolder/solder) with a new one. I could exactly programm it once as mentioned above -> then same error
5. Pulldown PA18 at startup in order to circumvent the BSL invokation -> same error
Has anything changed in CCS 20 in regard to Theia 1.5.1?
Thanks!
Best regards
Steffen