This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2634: Driving capacity of WARMRST# pin (C3) of AM2634

Part Number: AM2634

Tool/software:

Hi,

Do we have information on the driving capacity of WARMRST# pin (C3) of AM2634

Datasheet gives for other pins like RGMII, GPIOs, MMC etc, and all have little variations:

eg, min & max for RGMII pins is 3 pF / 25 pF
3 pF / 10 pF for GPIO
2 pF / 24 pF for SPI
5 pF / 20 pF for MCAN , etc