Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN
I am using a custom board tms570ls3137 with 16Mhz crytal.
AIthough I set up PLL1 and PLL2 the same but when I choose PLL1 for GCLK, the system work slower than PLL2.
With PLL2, I use rti to generate int at the rate of 1 Hz, clock source is 80Mhz and it blink ~= 4Hz period.
And when I choose OSC for GCLK, the system work 2 times slower than PLL 1.
Please give me a reason! Thanks.