Part Number: MSPM0G3519
Tool/software:
In the Mcal version-00.02.04.00, Pwm module was configured to use TIMG0 and TIMG14 to generate Pwm output, but when I changed the configuration from tresos to use TIMA0 it didn't work as expected.
And after some debugging it was found that timer instance array defined in Pwm_Priv.c which contains the base addresses for the timer instances was arranged in a different way than what was mentioned in the user guide, and also the function Pwm_Map_Timer_Instance_To_Map_Index which is defined in the same file.
So, as a result, when trying to use TIMA0 it was TIMG7 that actually got initialized and started the count.