Part Number: MSPM0G1506
Other Parts Discussed in Thread: MSPM0G3507
Tool/software:
Hi,
I managed to flash my application via UART BSL on the mspm0g3507 launchpad with default UART pins (Tx = PA 10, Rx = PA11).
But when I try to use my own board with non-default UART pins (Tx = PA 0, Rx = PA1) it fails. I changed wiring on one of my boards to default UART pins and it works.
Is the BSL only usable with default UART pins (Tx = PA 10, Rx = PA11)?
I understand I must use the default UART pins when I want to flash blank chips. But with an application running with configured non-default UART pins for BSL, it should work.
Thanks in advance
Matthias