Part Number: MSPM0G3507
Other Parts Discussed in Thread: DRV8323, DRV8316, DRV8328
Tool/software:
Hi there,
I am migrating a motor control project from C2000 to MSPM0G. I found the defined values of FULL_SCALE_CURRENT_BASE are not matched with the comments. Take DRV8323 for example, 3.3/2*(0.007*5) = 0.0578, not 11.785.
/*! @brief Full scale readable current used as current base value, calculated using (FULL Scale Voltage(3.3)/2*(Rsense(7mOhm) * CSA Gain(5)) */ #define FULL_SCALE_CURRENT_BASE 11.785
Also take DRV8316 for example, 3.3/2 * 0.15 = 0.248, not 11.
/*! @brief Full scale readable current used as current base value, calculated using (FULL Scale Voltage(3.3)/2* CSA Gain(0.15(v/A))) */ #define FULL_SCALE_CURRENT_BASE 11
According to the tuning guide, CURRENT_BASE = VREF / 2 / Gain(V/A).
For DRV8328: 3.3/2 / (0.007*5) = 47.143 ---> still not matched
For DRV8316: 3.3/2 / 0.15 = 11 ---> matched
These typos should be fixed.