Part Number: MSPM0G3507
Other Parts Discussed in Thread: DRV8329
Tool/software:
Hello my dear supporters and engineers,
I've asked several questions about driving a motor using MSPM0G3507 and DRV8329 using the code in "C:\ti\mspm0_sdk_2_02_00_05\examples\nortos\LP_MSPM0G3507\motor_control_pmsm_sensorless_foc\sensorless-foc_DRV8329", and now I'm at the step before the tuning step.
It seems. However, a critical problem was encountered.
According to the datasheet,




when using a 1m ohm shunt resistor, if R1 = 10k and R2 = 1k, CSAGAIN = 20, CURRENTBASE = 144.375. However, if the value is not 7.218 as written in the example code, the motor will not run. I would like to know what was violated in setting the currentbase.
If I change CSAGAIN to 40, it becomes 72.188, but this also does not work unless it is 7.218.
To follow the tuning guide, we first need to add Currentbase to the counter.
Please check this issue, and let me know if you need mor information.
Best regards,
Donguk