Part Number: LP-AM243
Tool/software:
Hi all,
I'm currently working with ethernetip_adapter_demo (ind_comms_sdk_am243x_09_02_00_08).
I configured the Predefined Symbols (project Properties → Build → Arm Compiler → Predefined Symbols: CPU_LOAD_MONITOR=1) to start the simple webserver.
Log on Terminal:
Pruicss max =3 selected PRU:3
PRU_PHY_detect:185 Phy 3 alive
PRU_PHY_detect:185 Phy 15 alive
Phy 3 : Disable RGMII mode
Phy 3 : Disable GBit ANEG
Phy 15 : Disable RGMII mode
Phy 15 : Disable GBit ANEG
+EI_API_ADP_pruicssStart
-EI_API_ADP_pruicssStart
Local interface IP is 192.168.1.10
EI_API_ADP_getMacAddr: 1c:63:49:25:1d:b5
pbuf_alloc failed on receiving nrt frame
pbuf_alloc failed on receiving nrt frame
pbuf_alloc failed on receiving nrt frame..
Connections tried:

Default configurations given to LP is
IP Address: 192.168.1.10
Network Mask: 255.255.255.0
Gateway Address: 192.168.1.1
Name Server: 0.0.0.0
So I have changed PC's EtherNet configuration to
IP Address: 192.168.1.20
Network Mask: 255.255.255.0
Gateway Address: 192.168.1.1
Connection 2:
Tried ping the IP 192.168.1.10 returns error
I didn't even receive single frame from the browser. Got only ARP frames in Wireshark.
Please guide me further
Regards,
D. Jenita.