Part Number: TMS570LS3137
Tool/software:
Asynchronous EMIF Port of the TMS570LS3137, try to write 1 byte data to a address (0x640000368), But the EMIF bus automatic send 5 Bytes to slave equipment, the address is from 0x368 to 0x36C
It seems like a alignment opperation.
C Code (*((volatile uint8*)(0x64000368U))) = (ucChkSum + 1U);
Disassembly Window in CCS: asm code : strb r12, [r13, #0x10]