Part Number: TMS570LC4357
Other Parts Discussed in Thread: CCSTUDIO
Tool/software:
Hi.
We just got a kit, TMS570LC43, and I wanted to test it out with one of the Hercules Safety MCU Demos.
We work in a 100% offline environment. Installed CCStudio 20.0.1 (after downloading and transferring to the offline computer)
When starting Code Composer Studio it is not able to identify the SDK/kit connected. "No compatible Board detected" Also the TMS570 is not listed in the dropdown "select a board or device"
The "Create new Project" appears to require to be online to function!
It only starts the wizard that state “Resource Explorer appears to be offline”
I have tried to reinstall, restart, noting works.
Using Uni_Flash i can read and write to the TMS570 kit so it is connected and working.
Any suggestions?