Part Number: TM4C123GH6PM
Tool/software:
Hi!!
I am trying to implement bootloader for TM4C123GH6PM at first i tried to make changes in the example project given in Tiva series (demo_serial example project) from UART0 to UART1 in bl_config.h file as shown and flashed the bin file tried to flash boot_demo1 using LM Flasher via UART but it is not flashing what might be the issue??? All the changes that i have made is configuring the UART from 0 to 1 but it is not working.
regards,
ANIL.
// Selects the clock enable for the UART peripheral module // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UARTx_BASE // //***************************************************************************** #define UART_CLOCK_ENABLE SYSCTL_RCGCUART_R1 //***************************************************************************** // // Selects the base address of the UART peripheral module // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_CLOCK_ENABLE // //***************************************************************************** #define UARTx_BASE UART1_BASE //***************************************************************************** // // Selects the clock enable for the GPIO corresponding to UART RX pin // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_RXPIN_BASE, UART_RXPIN_PCTL and UART_RXPIN_POS // //***************************************************************************** #define UART_RXPIN_CLOCK_ENABLE SYSCTL_RCGCGPIO_R2 //***************************************************************************** // // Selects the base address for the GPIO corresponding to UART RX pin // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_RXPIN_CLOCK_ENABLE, UART_RXPIN_PCTL and UART_RXPIN_POS // //***************************************************************************** #define UART_RXPIN_BASE GPIO_PORTC_BASE //***************************************************************************** // // Selects the port control value for the GPIO corresponding to UART RX pin // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_RXPIN_CLOCK_ENABLE, UART_RXPIN_BASE and UART_RXPIN_POS // //***************************************************************************** #define UART_RXPIN_PCTL 0x2 //***************************************************************************** // // Selects the pin number for the GPIO corresponding to UART RX pin // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_RXPIN_CLOCK_ENABLE, UART_RXPIN_BASE and UART_RXPIN_PCTL // //***************************************************************************** #define UART_RXPIN_POS 4 //***************************************************************************** // // Selects the clock enable for the GPIO corresponding to UART TX pin // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_TXPIN_BASE, UART_TXPIN_PCTL and UART_TXPIN_POS // //***************************************************************************** #define UART_TXPIN_CLOCK_ENABLE SYSCTL_RCGCGPIO_R2 //***************************************************************************** // // Selects the base address for the GPIO corresponding to UART TX pin // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_TXPIN_CLOCK_ENABLE, UART_TXPIN_PCTL and UART_TXPIN_POS // //***************************************************************************** #define UART_TXPIN_BASE GPIO_PORTC_BASE //***************************************************************************** // // Selects the port control value for the GPIO corresponding to UART TX pin // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_TXPIN_CLOCK_ENABLE, UART_TXPIN_BASE and UART_TXPIN_POS // //***************************************************************************** #define UART_TXPIN_PCTL 0x2 //***************************************************************************** // // Selects the pin number for the GPIO corresponding to UART TX pin // // Depends on: UART_ENABLE_UPDATE // Exclusive of: None // Requires: UART_TXPIN_CLOCK_ENABLE, UART_TXPIN_BASE and UART_TXPIN_PCTL // //***************************************************************************** #define UART_TXPIN_POS 5 //*****************************************************************************
Thanks for your reply Charles!!!