Part Number: LP-AM243
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi there,
I am running an ethercat slave application on core 0-0 and a motor control application on core 1-0. But due to the following bug, when I run core 1-0 after core 0-0, core 0-0 does not work properly, when I run core 0-0 after core 1-0, this time core motor application on core 1-0 doies not work properly.
SDK Bug:
MCUSDK-12117 Setting the ICSSG1 clock frequency affects the ICSSG0 clock frequency.
The error occured when I passed on System_init function. It initializes ICSG defined in sysconfig file and it affects other core's ICSG clock frequency. Core 0-0 has 300Mhz ICSG freq and core 1-0 has 200.
I use motor_control_sdk_am243x_09_02_00_09 version of motor control sdk, and MCU plus SDK that I am using is included inside motor control SDK.
Can I solve this problem if I upgrade my SDK version? Which SDK versions should I use?
Regads
Kadir