Part Number: MSPM0G3507
Tool/software:
Hello,
I've found this thread about issues with MSPM0G3507 SVD: https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1398791/mspm0g3507-could-you-provide-svd-files-for-mspm0g3xxx-family
I'm attempting to compile TI's provided MSPM0G3507 SVD by svd2rust compiler in order to be able to use the MCU with Rust. Anyway, so far I've just replaced all 'read-writeonce' with `read-write' and also did this change:
@@ -74984,7 +74984,7 @@
<description>Bank not in read mode.
Indicates which banks are not in READ mode. There is 1 bit per bank.</description>
<bitOffset>0x0</bitOffset>
- <bitWidth>0x1</bitWidth>
+ <bitWidth>0x5</bitWidth>
<access>read-only</access>
<enumeratedValues>
<enumeratedValue>
in order to have Rust code produced from the SVD file.
Anyway, still I do have issues where some registers are missing from the generated code. So far I'm concentrating on ass imple as possible "blinking LED" example hence with just GPIO. The SVD GPIO definitions provide several registers defined in 'cluster'. Unfortunately this does not work well with my svd2rust and I get no code produced for those registers.
It may be just an issue with my svd2rust (0.35.0, latest release as of today), but what is interesting is that TI itself has changed problematic code (involving clusters) in MSPM0L130X.svd. In 2023 version (the file distributed as part of VS Code Cortex-Debug extension) the SVD file contains register clusters while latest code from TI rewrites this to use non-closter register sequence. The diff of header should be helpfull in order to identify the changes I'm talking here:
--- MSPM0L130X.svd 2024-05-24 13:59:22.000000000 +0200
+++ /c/Users/gardas/git/SE/TI_MSPM0L/mspm0l130x/MSPM0L130X.svd 2024-12-12 19:33:15.692204100 +0100
@@ -1,12 +1,12 @@
-<?xml version="1.0" encoding="utf-8"?>
-<device schemaVersion="1.2" xmlns:xs="http://www.w3.org/2001/XMLSchema-instance" xs:noNamespaceSchemaLocation="CMSIS-SVD.xsd" >
+<?xml version='1.0' encoding='UTF-8'?>
+<device xmlns:xs="http://www.w3.org/2001/XMLSchema-instance" schemaVersion="1.2" xs:noNamespaceSchemaLocation="CMSIS-SVD.xsd">
<vendor>Texas Instruments</vendor>
<vendorID>ti.com</vendorID>
<name>MSPM0L130X</name>
- <version>This preliminary header file does not have a version number - build date: 2024-04-29 21:56:11</version>
+ <version>This preliminary header file does not have a version number - build date: 2023-02-21 16:43:37</version>
<description>ARM Device</description>
<licenseText>
- Copyright (C) 2024 Texas Instruments Incorporated - http://www.ti.com/
+ Copyright (C) 2023 Texas Instruments Incorporated - http://www.ti.com/
Now, while seeing this MSP-L series SVD definition change I'm curious if TI is planning to do similar change in G-series SVD files?
Thanks!
Karel