Part Number: MSPM0G1507
Other Parts Discussed in Thread: LP-MSPM0G3507
Tool/software:
I am working on a demo utilizing the LP-MSPM0G3507 (For the MSPM0G1507) trying to understand the maximum amount of PWM Channels I can utilize to interface with 3 different motor drivers.
The data sheet says the following:
Seven timers supports up to 22 PWM channels
• One 16-bit general-purpose timer
• One 16-bit general-purpose timer supports QEI
• Two 16-bit general-purpose timers support low-power operation in STANDBY mode
• One 32-bit high-resolution general-purpose timer
• Two 16-bit advanced timers with deadband support up to 12 PWM channels
What is the limit for how many of these can be configured for the LP-MSPM0G3507 for a demo? What limitations are there? (I.e. if I am configuring 2 channels under PWM_0, do they need to be configured for the same PWM duty cycle, etc)