Part Number: TM4C1294NCPDT
Tool/software:
Im trying to follow this note form the datasheet,
"if the SSIClk signal is programmed to steady state High through the SPO bit in the SSICR0 register, then software must also configure the GPIO port pin corresponding to the SSInClk signal as a pull-up in the GPIO Pull-Up Select (GPIOPUR) register."
These lines did not give me the desired result, the GPIOPUR regitser sets the bit 0 and it gets reset to 0 on the next lines of code.
GPIOUnlockPin(GPIO_PORTQ_BASE, GPIO_PIN_0); //unlock the pin for write access to commit reg
GPIOPadConfigSet(GPIO_PORTQ_BASE, GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
I have also tried by manipulating registers directly,
HWREG(GPIO_PORTQ_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTQ_BASE + GPIO_O_CR) |= GPIO_PIN_0;
HWREG(GPIO_PORTQ_BASE + GPIO_O_PUR) |= GPIO_PIN_0;
This is snippet from SPI Module intialisation which is configured to mode 3, SPO =1, SPH = 1.
complete code,
void clock_init(){
ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_CFG_VCO_160),40000000);
}
void SPI_init(){
/*
* 360 NW uses the SSI3 Module of TM4CNCPDT controller
* By default only SPI mode can be used in SST26VF032B SPI flash
* SST26VF032B/SST26VF032BA -> MAX CLOCK 104 MHz / 80 MHz
*/
clock_init();
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOQ)); //wait for enable
GPIOPinConfigure(GPIO_PQ0_SSI3CLK);
GPIOPinConfigure(GPIO_PQ1_SSI3FSS);
GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0); //Tx
GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1); //Rx
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_SSI3)); //wait for enable
GPIOUnlockPin(GPIO_PORTQ_BASE, GPIO_PIN_0); //unlock the pin for write access to commit reg
// Unlock the port by using the device LOCK key
//
// HWREG(GPIO_PORTQ_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
//
// //
// // Commit the pin to keep it in GPIO mode
// //
// HWREG(GPIO_PORTQ_BASE + GPIO_O_CR) |= GPIO_PIN_0;
//
// HWREG(GPIO_PORTQ_BASE + GPIO_O_PUR) |= GPIO_PIN_0;
// to ensure clock is sharp for falling edge, since sck is pulled up in Spi flash
GPIOPadConfigSet(GPIO_PORTQ_BASE, GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
GPIOPinTypeSSI(GPIO_PORTQ_BASE,GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
SSIConfigSetExpClk(SSI3_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_3, SSI_MODE_MASTER, 10000000, 8);
SSIEnable(SSI3_BASE);
}
How to solve this?