Part Number: LP-MSPM0G3519
Other Parts Discussed in Thread: MSPM0G3519, SYSCONFIG
Tool/software:
What is the maximum possible PWM frequency can be generated, and max frequency can be capture using MSPM0G3519 controller?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-MSPM0G3519
Other Parts Discussed in Thread: MSPM0G3519, SYSCONFIG
Tool/software:
What is the maximum possible PWM frequency can be generated, and max frequency can be capture using MSPM0G3519 controller?
Hi Rohidas,
It will depend on the Time Clock Source, the Timer Peripheral, and the PWM Period Count. The maximum frequency you can reach can be modified in the Clock Tree in SYSCONFIG (keep in mind that ULPCLK's maximum supported frequency is 40MHz.) Normally, the frequency source is 32MHz.
Best Regards,
Diego Abad