Tool/software:
Hi,
As it seems that the following thread was locked, let me ask the same question here.
AM243x got SIL2 certification.
https://www.ti.com/jp/lit/pdf/sffs846
Is that assumed to use some of diagnostic function in the safety island (MCU Island) ?
Or it doesn’t depend on the use of the features in the safety island ?
For example, is SIL2 certification valid in the case of even only R5F core is used without Safety Island ?
The customer has to explain the above for getting the certification of their system with AM2431.
Please provide your comment. It would be appreciated if we can receive it as soon as possible.
Thanks and regards,
Hideaki