Part Number: MSPM0L2228
Tool/software:
I am using CCS 20.0.1 with the MSPM0L2228.
I upgraded from CCS Theia 1.5.1 to CCS 20.0.1 last week, and everything seemed to be working fine.
I did notice a firmware update of the XDS110 debug probe was done when I first ran CCS 20.0.1.
I have made some small code changes to my project, and now it is not possible to run that project, or any other I have ran over the previous two months.
Without altering any other project, they all result in the same problem, main is not reached, and the code ends up in the Default_Handler:

Reverting my recent changes back too, and still the same problem.
I have tried CCS Theia 1.5.1 again as well, and still the same problem.
I am at a bit of a loss as to what to try next, and just do not understand what has happened from working fine last week, no apparent changes since upgrading to CCS 20.0.1 and now cannot debug at all.