Part Number: MSPM0G3507
Other Parts Discussed in Thread: OPA2365, UNIFLASH, , SYSCONFIG
Tool/software:
Hi,
I got this message when trying to flash a MCU MSPM03507.

And I see this relevant post:
Tried to 1) hold S1 (I thinks S2 is typo) and flash, 2) hold S1 and press then release RESET, and then flash, no one works to address this issue. J8 is connected. And tried to keep NRST on J101 connected or populated, still not working in both cases.
My understanding is that this device's non-main memory needs to be erased, right?
Then the issue will gone with non-main memory empty? I would like to confirm the process before going ahead to erase non-main memory.
In addition, at the end it says "so please make sure that is not selected: ". It means normally "erase main and nonmain memory" should not be selected, right?
Thanks!
Crane