Part Number: AM263P4-Q1
Tool/software:
Dear Sir/Madam,
I am currently working on the MCAN peripheral of the AM263Px CC. I am using a modified version of the mcan_external_read_write example from the AM263Px MCU+SDK (Version 10.01.00.31) to enable the transmission and reception of Extended CAN ID messages.
I have written a condition in the code such that data bytes are transmitted only when the rxMsg_id matches a specific condition. This ensures that the transmission is based solely on the matching of the received CAN ID (rxMsg_id), irrespective of the matching of data bytes from the received message.
However, I am encountering the following issues:
- Even though the CAN message being sent has an ID that matches the condition in the code, the condition is not being entered during execution.
- During debugging through UART logs, the system consistently treats the received ID as
0x70043E80by default, irrespective of the actual received ID.
To aid in diagnosing the issue, I have attached the following for your reference:
- The code I am working with.
- Debug logs captured during execution.
Could you please assist in identifying the root cause of these issues and provide guidance on how to resolve them?
Thank you for your support.
Kind regards,
Tarun
/*
* Copyright (C) 2023 Texas Instruments Incorporated
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/* This example demonstrates the CAN message communication to external CAN
* controller in with the following configuration.
* CAN FD Message Format.
* Message ID Type is Standard, Msg Id 0xC0.
* MCAN is configured in Interrupt Mode.
* MCAN Interrupt Line Number 0.
* Arbitration Bit Rate 1Mbps.
* Data Bit Rate 5Mbps.
* Buffer mode is used for Tx and RX to store message in message RAM.
* Instance MCAN1 is set as a Commander in Transmit Mode. Message is transmitted and received
* back from external CAN controller. Once message is transmitted the example will wait for
* recieving the messages from external PC. Have to manually transmit ten messages from external
* PC for test to finish. When the received message id and the data matches with the transmitted
* one, then the example is completed.
*/
//#include <cstdint>
#include <stdio.h>
#include <kernel/dpl/DebugP.h>
#include <kernel/dpl/AddrTranslateP.h>
#include <kernel/dpl/SemaphoreP.h>
#include <drivers/mcan.h>
#include "drivers/mcan/v0/hw_mcanss.h"
#include "ti_drivers_config.h"
#include "ti_drivers_open_close.h"
#include "ti_board_open_close.h"
#define APP_MCAN_BASE_ADDR (CONFIG_MCAN0_BASE_ADDR)
#define APP_MCAN_INTR_NUM (CONFIG_MCAN0_INTR)
#define APP_MCAN_MSG_LOOP_COUNT (1U)
#define APP_MCAN_LOOPBACK_MODE_DISABLE (TRUE)
/* Allocate Message RAM memory section to filter elements, buffers, FIFO */
/* Maximum STD Filter Element can be configured is 128 */
#define APP_MCAN_STD_ID_FILTER_CNT (0U)
/* Maximum EXT Filter Element can be configured is 64 */
#define APP_MCAN_EXT_ID_FILTER_CNT (1U)
/* Maximum TX Buffer + TX FIFO, combined can be configured is 32 */
#define APP_MCAN_TX_BUFF_CNT (1U)
#define APP_MCAN_TX_FIFO_CNT (0U)
/* Maximum TX Event FIFO can be configured is 32 */
#define APP_MCAN_TX_EVENT_FIFO_CNT (0U)
/* Maximum RX FIFO 0 can be configured is 64 */
#define APP_MCAN_FIFO_0_CNT (0U)
/* Maximum RX FIFO 1 can be configured is 64 and
* rest of the memory is allocated to RX buffer which is again of max size 64 */
#define APP_MCAN_FIFO_1_CNT (0U)
/* Standard Id configured in this app */
//#define APP_MCAN_STD_ID (0xC0U)
//#define APP_MCAN_STD_ID_MASK (0x7FFU)
//#define APP_MCAN_STD_ID_SHIFT (18U)
#define APP_MCAN_EXT_ID (0x123FU)
#define APP_MCAN_EXT_ID1 (0x456FU)
#define APP_MCAN_EXT_ID_MASK (0x1FFFFFFFU)
#define APP_MCAN_EXT_ID_SHIFT (0U)
/* In the CAN FD format, the Data length coding differs from the standard CAN.
* In case of standard CAN it is 8 bytes */
static uint8_t gMcanDataSize[16U] = {0U, 1U, 2U, 3U,
4U, 5U, 6U, 7U,
8U, 12U, 16U, 20U,
24U, 32U, 48U, 64U};
/* Semaphore to indicate transfer completion */
static SemaphoreP_Object gMcanTxDoneSem, gMcanRxDoneSem;
static HwiP_Object gMcanHwiObject;
static uint32_t gMcanBaseAddr;
/* Static Function Declarations */
static void App_mcanIntrISR(void *arg);
static void App_mcanConfig(Bool enableExternalLpbk);
static void App_mcanInitMsgRamConfigParams(
MCAN_MsgRAMConfigParams *msgRAMConfigParams);
static void App_mcanEnableIntr(void);
//static void App_mcanConfigTxMsg(MCAN_TxBufElement *txMsg);
static void App_mcanConfigTxMsg(MCAN_TxBufElement *txMsg, MCAN_RxBufElement *rxMsg);
static void App_mcanCompareMsg(MCAN_TxBufElement *txMsg,
MCAN_RxBufElement *rxMsg);
static void App_mcanInitExtFilterElemParams(
MCAN_ExtMsgIDFilterElement *extFiltElem,
uint32_t bufNum);
static bool test_flag = TRUE;
void mcanEnableTransceiver(void);
void mcan_external_read_write_main(void *args)
{
int32_t status = SystemP_SUCCESS;
HwiP_Params hwiPrms;
MCAN_TxBufElement txMsg;
MCAN_ProtocolStatus protStatus;
MCAN_RxBufElement rxMsg;
MCAN_RxNewDataStatus newDataStatus;
MCAN_ErrCntStatus errCounter;
uint32_t i, bufNum, fifoNum, bitPos = 0U;
/* Open drivers to open the UART driver for console */
Drivers_open();
Board_driversOpen();
mcanEnableTransceiver();
DebugP_log("[MCAN] External read - write test, application started ...\r\n");
/* Construct Tx/Rx Semaphore objects */
status = SemaphoreP_constructBinary(&gMcanTxDoneSem, 0);
DebugP_assert(SystemP_SUCCESS == status);
status = SemaphoreP_constructBinary(&gMcanRxDoneSem, 0);
DebugP_assert(SystemP_SUCCESS == status);
/* Register interrupt */
HwiP_Params_init(&hwiPrms);
hwiPrms.intNum = APP_MCAN_INTR_NUM;
hwiPrms.callback = &App_mcanIntrISR;
status = HwiP_construct(&gMcanHwiObject, &hwiPrms);
DebugP_assert(status == SystemP_SUCCESS);
/* Assign MCAN instance address */
gMcanBaseAddr = (uint32_t) AddrTranslateP_getLocalAddr(APP_MCAN_BASE_ADDR);
/* Configure MCAN module, Enable External LoopBack Mode */
App_mcanConfig(APP_MCAN_LOOPBACK_MODE_DISABLE);
/* Enable Interrupts */
App_mcanEnableIntr();
DebugP_log("After transmitting the messages, it will wait to recieve ten messages for test to pass ...\r\n");
/* Transmit And Receive Message */
// for (i = 0U; i < APP_MCAN_MSG_LOOP_COUNT; i++)
// {
/* Configure Tx Msg to transmit */
// App_mcanConfigTxMsg(&txMsg);
App_mcanConfigTxMsg(&txMsg, &rxMsg);
/* Select buffer number, 32 buffers available */
bufNum = 0U;
/* Enable Transmission interrupt for the selected buf num,
* If FIFO is used, then need to send FIFO start index until FIFO count */
status = MCAN_txBufTransIntrEnable(gMcanBaseAddr, bufNum, (uint32_t)TRUE);
DebugP_assert(status == CSL_PASS);
/* Write message to Msg RAM */
MCAN_writeMsgRam(gMcanBaseAddr, MCAN_MEM_TYPE_BUF, bufNum, &txMsg);
/* Add request for transmission, This function will trigger transmission */
status = MCAN_txBufAddReq(gMcanBaseAddr, bufNum);
DebugP_assert(status == CSL_PASS);
/* Wait for Tx completion */
SemaphoreP_pend(&gMcanTxDoneSem, SystemP_WAIT_FOREVER);
MCAN_getProtocolStatus(gMcanBaseAddr, &protStatus);
/* Checking for Tx Errors */
if (((MCAN_ERR_CODE_NO_ERROR != protStatus.lastErrCode) ||
(MCAN_ERR_CODE_NO_CHANGE != protStatus.lastErrCode)) &&
((MCAN_ERR_CODE_NO_ERROR != protStatus.dlec) ||
(MCAN_ERR_CODE_NO_CHANGE != protStatus.dlec)) &&
(0U != protStatus.pxe))
{
DebugP_assert(FALSE);
}
/* Wait for Rx completion */
SemaphoreP_pend(&gMcanRxDoneSem, SystemP_WAIT_FOREVER);
/* Checking for Rx Errors */
MCAN_getErrCounters(gMcanBaseAddr, &errCounter);
DebugP_assert((0U == errCounter.recErrCnt) &&
(0U == errCounter.canErrLogCnt));
/* Get the new data staus, indicates buffer num which received message */
MCAN_getNewDataStatus(gMcanBaseAddr, &newDataStatus);
MCAN_clearNewDataStatus(gMcanBaseAddr, &newDataStatus);
/* Select buffer and fifo number, Buffer is used in this app */
bufNum = 0U;
fifoNum = MCAN_RX_FIFO_NUM_0;
bitPos = (1U << bufNum);
if (bitPos == (newDataStatus.statusLow & bitPos))
{
MCAN_readMsgRam(gMcanBaseAddr, MCAN_MEM_TYPE_BUF, bufNum, fifoNum, &rxMsg);
}
else
{
DebugP_assert(FALSE);
}
/* Compare Tx/Rx data */
// App_mcanCompareMsg(&txMsg, &rxMsg);
// }
/* De-Construct Tx/Rx Semaphore objects */
HwiP_destruct(&gMcanHwiObject);
SemaphoreP_destruct(&gMcanTxDoneSem);
SemaphoreP_destruct(&gMcanRxDoneSem);
MCAN_reset(gMcanBaseAddr);
DebugP_log("All tests have passed!!\r\n");
Board_driversClose();
Drivers_close();
return;
}
static void App_mcanConfig(Bool enableExternalLpbk)
{
MCAN_ExtMsgIDFilterElement extFiltElem[APP_MCAN_EXT_ID_FILTER_CNT] = {0U};
MCAN_InitParams initParams = {0U};
MCAN_ConfigParams configParams = {0U};
MCAN_MsgRAMConfigParams msgRAMConfigParams = {0U};
MCAN_BitTimingParams bitTimes = {0U};
uint32_t i;
/* Initialize MCAN module initParams */
MCAN_initOperModeParams(&initParams);
/* CAN FD Mode and Bit Rate Switch Enabled */
initParams.fdMode = FALSE;
initParams.brsEnable = FALSE;
/* Initialize MCAN module Global Filter Params */
MCAN_initGlobalFilterConfigParams(&configParams);
/* Initialize MCAN module Bit Time Params */
/* Configuring default 1Mbps and 5Mbps as nominal and data bit-rate resp */
MCAN_initSetBitTimeParams(&bitTimes);
/* Initialize MCAN module Message Ram Params */
App_mcanInitMsgRamConfigParams(&msgRAMConfigParams);
/* Initialize Filter element to receive msg, should be same as tx msg id */
for (i = 0U; i < APP_MCAN_EXT_ID_FILTER_CNT; i++)
{
App_mcanInitExtFilterElemParams(&extFiltElem[i], i);
}
/* wait for memory initialization to happen */
while (FALSE == MCAN_isMemInitDone(gMcanBaseAddr))
{}
/* Put MCAN in SW initialization mode */
MCAN_setOpMode(gMcanBaseAddr, MCAN_OPERATION_MODE_SW_INIT);
while (MCAN_OPERATION_MODE_SW_INIT != MCAN_getOpMode(gMcanBaseAddr))
{}
/* Initialize MCAN module */
MCAN_init(gMcanBaseAddr, &initParams);
/* Configure MCAN module Gloabal Filter */
MCAN_config(gMcanBaseAddr, &configParams);
/* Configure Bit timings */
MCAN_setBitTime(gMcanBaseAddr, &bitTimes);
/* Configure Message RAM Sections */
MCAN_msgRAMConfig(gMcanBaseAddr, &msgRAMConfigParams);
/* Set Extended ID Mask */
MCAN_setExtIDAndMask(gMcanBaseAddr, APP_MCAN_EXT_ID_MASK);
/* Configure Standard ID filter element */
for (i = 0U; i < APP_MCAN_EXT_ID_FILTER_CNT; i++)
{
MCAN_addExtMsgIDFilter(gMcanBaseAddr, i, &extFiltElem[i]);
}
if (TRUE == enableExternalLpbk)
{
MCAN_lpbkModeEnable(gMcanBaseAddr, MCAN_LPBK_MODE_EXTERNAL, FALSE);
}
/* Take MCAN out of the SW initialization mode */
MCAN_setOpMode(gMcanBaseAddr, MCAN_OPERATION_MODE_NORMAL);
while (MCAN_OPERATION_MODE_NORMAL != MCAN_getOpMode(gMcanBaseAddr))
{}
return;
}
static void App_mcanConfigTxMsg(MCAN_TxBufElement *txMsg, MCAN_RxBufElement *rxMsg)
{
uint32_t i;
uint8_t cantx_buf[8] = {0x0A, 0x92, 0x3F, 0x67, 0xD4, 0xC5, 0x88, 0xB7};
uint8_t canrx_buf[8] = {0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F, 0x07, 0x08};
/* Initialize message to transmit */
MCAN_initTxBufElement(txMsg);
/* Standard message identifier 11 bit, stored into ID[28-18] */
txMsg->id = ((APP_MCAN_EXT_ID & MCAN_EXT_ID_MASK) << MCAN_EXT_ID_SHIFT);
txMsg->dlc = MCAN_DATA_SIZE_8BYTES; /* Payload size is 64 bytes */
txMsg->fdf = FALSE; /* CAN FD Frame Format */
txMsg->xtd = TRUE; /* Extended id not configured */
if (test_flag == TRUE)
{
for (i = 0U; i < MCAN_DATA_SIZE_8BYTES; i++)
{
txMsg->data[i] = cantx_buf[i];
DebugP_log("txMsg->data[%d]: %d\r\n",i,txMsg->data[i]);
DebugP_log("txMsg->id: %d (0x%X)\r\n", txMsg->id, txMsg->id);
DebugP_log("rxMsg->id: %d (0x%X)\r\n", rxMsg->id, rxMsg->id);
}
test_flag = FALSE;
}
if (((txMsg->id >> MCAN_EXT_ID_SHIFT) & MCAN_EXT_ID_MASK) ==
((rxMsg->id >> MCAN_EXT_ID_SHIFT) & MCAN_EXT_ID_MASK))
{
//txMsg->id = ((0x101FU & MCAN_EXT_ID_MASK) << MCAN_EXT_ID_SHIFT);
for (i = 0U; i < MCAN_DATA_SIZE_8BYTES; i++)
{
txMsg->data[i] = canrx_buf[i];
DebugP_log("txMsg->data[%d]: %d\r\n",i,txMsg->data[i]);
DebugP_log("txMsg->id: %d (0x%X)\r\n", txMsg->id, txMsg->id);
DebugP_log("rxMsg->id: %d (0x%X)\r\n", rxMsg->id, rxMsg->id);
DebugP_log("txMsg->dlc: %d\r\n", txMsg->dlc);
DebugP_log("txMsg->xtd: %d\r\n", txMsg->xtd);
DebugP_log("txMsg->fdf: %d\r\n", txMsg->fdf);
DebugP_log("MCAN_EXT_ID_MASK: 0x%X\r\n", MCAN_EXT_ID_MASK);
DebugP_log("MCAN_EXT_ID_SHIFT: %d\r\n", MCAN_EXT_ID_SHIFT);
}
}
return;
}
static void App_mcanInitExtFilterElemParams(MCAN_ExtMsgIDFilterElement *extFiltElem,
uint32_t bufNum)
{
/* sfid1 defines the ID of the standard message to be stored. */
extFiltElem->efid1 = APP_MCAN_EXT_ID;
/* As buffer mode is selected, sfid2 should be bufNum[0 - 63] */
extFiltElem->efid2 = bufNum;
/* Store message in buffer */
extFiltElem->efec = MCAN_EXT_FILT_ELEM_BUFFER;
/* Below configuration is ignored if message is stored in buffer */
extFiltElem->eft = MCAN_EXT_FILT_TYPE_RANGE;
return;
}
/*static void App_mcanInitExtFilterElemParams(MCAN_ExtMsgIDFilterElement *extFiltElem,
uint32_t bufNum)
{
static const uint32_t ext_ids[] = {0x101F, 0x201F, 0x301F};
static uint8_t current_id_index = 0; // Variable to keep track of the current ID being used
extFiltElem->efid1 = (ext_ids[current_id_index] & MCAN_EXT_ID_MASK) << MCAN_EXT_ID_SHIFT;
extFiltElem->efid2 = bufNum;
extFiltElem->efec = MCAN_EXT_FILT_ELEM_BUFFER;
extFiltElem->eft = MCAN_EXT_FILT_TYPE_RANGE;
current_id_index = (current_id_index + 1) % 3; // Cycle through the 3 IDs (0x101F, 0x201F, 0x301F)
return;
}
*/
static void App_mcanEnableIntr(void)
{
MCAN_enableIntr(gMcanBaseAddr, MCAN_INTR_MASK_ALL, (uint32_t)TRUE);
MCAN_enableIntr(gMcanBaseAddr,
MCAN_INTR_SRC_RES_ADDR_ACCESS, (uint32_t)FALSE);
/* Select Interrupt Line 0 */
MCAN_selectIntrLine(gMcanBaseAddr, MCAN_INTR_MASK_ALL, MCAN_INTR_LINE_NUM_0);
/* Enable Interrupt Line */
MCAN_enableIntrLine(gMcanBaseAddr, MCAN_INTR_LINE_NUM_0, (uint32_t)TRUE);
return;
}
static void App_mcanInitMsgRamConfigParams(MCAN_MsgRAMConfigParams
*msgRAMConfigParams)
{
int32_t status;
MCAN_initMsgRamConfigParams(msgRAMConfigParams);
/* Configure the user required msg ram params */
msgRAMConfigParams->lss = APP_MCAN_STD_ID_FILTER_CNT;
msgRAMConfigParams->lse = APP_MCAN_EXT_ID_FILTER_CNT;
msgRAMConfigParams->txBufCnt = APP_MCAN_TX_BUFF_CNT;
msgRAMConfigParams->txFIFOCnt = APP_MCAN_TX_FIFO_CNT;
/* Buffer/FIFO mode is selected */
msgRAMConfigParams->txBufMode = MCAN_TX_MEM_TYPE_BUF;
msgRAMConfigParams->txEventFIFOCnt = APP_MCAN_TX_EVENT_FIFO_CNT;
msgRAMConfigParams->rxFIFO0Cnt = APP_MCAN_FIFO_0_CNT;
msgRAMConfigParams->rxFIFO1Cnt = APP_MCAN_FIFO_1_CNT;
/* FIFO blocking mode is selected */
msgRAMConfigParams->rxFIFO0OpMode = MCAN_RX_FIFO_OPERATION_MODE_BLOCKING;
msgRAMConfigParams->rxFIFO1OpMode = MCAN_RX_FIFO_OPERATION_MODE_BLOCKING;
status = MCAN_calcMsgRamParamsStartAddr(msgRAMConfigParams);
DebugP_assert(status == CSL_PASS);
return;
}
static void App_mcanCompareMsg(MCAN_TxBufElement *txMsg,
MCAN_RxBufElement *rxMsg)
{
// uint32_t i;
if (((txMsg->id >> APP_MCAN_EXT_ID_SHIFT) & APP_MCAN_EXT_ID_MASK) !=
((rxMsg->id >> APP_MCAN_EXT_ID_SHIFT) & APP_MCAN_EXT_ID_MASK))
{
DebugP_logError("Message ID mismatch !!!\r\n");
DebugP_assert(FALSE);
//for (i = 0U; i < gMcanDataSize[MCAN_DATA_SIZE_8BYTES]; i++)
//{
// if (txMsg->data[i] != rxMsg->data[i])
//{
//DebugP_logError("Data mismatch !!!\r\n");
//DebugP_assert(FALSE);
// }
//}
}
else
{
;
}
return;
}
static void App_mcanIntrISR(void *arg)
{
uint32_t intrStatus;
intrStatus = MCAN_getIntrStatus(gMcanBaseAddr);
MCAN_clearIntrStatus(gMcanBaseAddr, intrStatus);
if (MCAN_INTR_SRC_TRANS_COMPLETE ==
(intrStatus & MCAN_INTR_SRC_TRANS_COMPLETE))
{
SemaphoreP_post(&gMcanTxDoneSem);
}
/* If FIFO0/FIFO1 is used, then MCAN_INTR_SRC_DEDICATED_RX_BUFF_MSG macro
* needs to be replaced by MCAN_INTR_SRC_RX_FIFO0_NEW_MSG/
* MCAN_INTR_SRC_RX_FIFO1_NEW_MSG respectively */
if (MCAN_INTR_SRC_DEDICATED_RX_BUFF_MSG ==
(intrStatus & MCAN_INTR_SRC_DEDICATED_RX_BUFF_MSG))
{
SemaphoreP_post(&gMcanRxDoneSem);
}
return;
}
Cortex_R5_0: [MCAN] External read - write test, application started ... Cortex_R5_0: After transmitting the messages, it will wait to recieve ten messages for test to pass ... Cortex_R5_0: txMsg->data[0]: 10 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[1]: 146 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[2]: 63 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[3]: 103 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[4]: 212 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[5]: 197 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[6]: 136 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[7]: 183 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[0]: 10 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[1]: 11 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[2]: 12 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[3]: 13 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[4]: 14 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[5]: 15 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[6]: 7 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[7]: 8 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: All tests have passed!! Cortex_R5_0: [MCAN] External read - write test, application started ... Cortex_R5_0: After transmitting the messages, it will wait to recieve ten messages for test to pass ... Cortex_R5_0: txMsg->data[0]: 10 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[1]: 11 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[2]: 12 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[3]: 13 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[4]: 14 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[5]: 15 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[6]: 7 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[7]: 8 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: All tests have passed!! Cortex_R5_0: [MCAN] External read - write test, application started ... Cortex_R5_0: After transmitting the messages, it will wait to recieve ten messages for test to pass ... Cortex_R5_0: txMsg->data[0]: 10 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[1]: 11 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[2]: 12 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[3]: 13 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[4]: 14 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[5]: 15 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[6]: 7 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[7]: 8 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: [MCAN] External read - write test, application started ... Cortex_R5_0: After transmitting the messages, it will wait to recieve ten messages for test to pass ... Cortex_R5_0: txMsg->data[0]: 10 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[1]: 146 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[2]: 63 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[3]: 103 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[4]: 212 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[5]: 197 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[6]: 136 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->data[7]: 183 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: All tests have passed!! Cortex_R5_0: [MCAN] External read - write test, application started ... Cortex_R5_0: After transmitting the messages, it will wait to recieve ten messages for test to pass ... Cortex_R5_0: txMsg->data[0]: 10 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[1]: 11 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[2]: 12 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[3]: 13 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[4]: 14 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[5]: 15 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[6]: 7 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[7]: 8 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: All tests have passed!! Cortex_R5_0: [MCAN] External read - write test, application started ... Cortex_R5_0: After transmitting the messages, it will wait to recieve ten messages for test to pass ... Cortex_R5_0: txMsg->data[0]: 10 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[1]: 11 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[2]: 12 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[3]: 13 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[4]: 14 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[5]: 15 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[6]: 7 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0 Cortex_R5_0: txMsg->data[7]: 8 Cortex_R5_0: txMsg->id: 4671 (0x123F) Cortex_R5_0: rxMsg->id: 4671 (0x70043E80) Cortex_R5_0: txMsg->dlc: 8 Cortex_R5_0: txMsg->xtd: 1 Cortex_R5_0: txMsg->fdf: 0 Cortex_R5_0: MCAN_EXT_ID_MASK: 0x1FFFFFFF Cortex_R5_0: MCAN_EXT_ID_SHIFT: 0