Part Number: TMS570LC4357
Tool/software:
Hello,
If it is not under NDA, could you please explain the rationale behind the following note in the TMS570 TRM (SPNU563A–March 2018 , page 144) ?
"NOTE: Selecting a clock source for RTICLK1 that is not VCLK When the application chooses a clock source for the RTICLK1 domain that is not VCLK, then the application must ensure that the resulting RTICLK1 frequency is less than or equal to the VCLK frequency divided by 3. The application can configure the RTI1DIV field of the RCLKSRC register to divide the selected clock source frequency by 1, 2, 4, or 8 to meet this requirement."
Specifically, what is the reason for this requirement, and what could potentially happen if the RTI clock frequency is set to be greater than the VCLK frequency divided by 3?
Thank you.