Part Number: MSPM0G3507-Q1
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi guys,
we build a new prototype board with MSPM0G3507-Q1. We want to use an external 24 MHz crytal. I did not saw any requirements for the choice of the crystal in the HW Design guide, like drive level etc.
We use the XRCGE24M000FBA1AR0 from Murata with the following Caps

Are there no requirements for this MCU regarding to the crystal like drive level?
We have the following problem if I configure the Clock tree in CCS with the following configuration



and activate it in SYSCTL

I can flash the MCU one time and then i get the following error

Trouble Writing Register PC: Error occured in writeRegister()!.
When I try to flash a second time then it is not flashable and the Debug Output brings the following message

We flash with Segger JLINK. When i just use the internal oscillator I have no problems, but the crystal does not go hot or anything.
I then have to unsolder the MCU because I don't know how to restore it to its original state. I think the controller is not damaged just in an unflashable state.
I look forward to hearing from you soon.
Thanks.
Kind regards
Dominik Maier