Part Number: TMS570LC4357
Tool/software:
Hi,
I have read the post titled: TMS570LC4357: WDT handling - upon watchdog reset
I am using the watchdog in the following way:
void startWatchDog(void)
{
/*watch dog*/
dwdInit(WDOG_REG, WDOG_TIMEOUT); //set pre scaler and timer to use
dwdCounterEnable(WDOG_REG); //turn on
}
/*************************************************************************************
* Function name : petWatchdog()
* Description : reset the watch dog
*
* @return - nothing
***************************************************************************************/
void petWatchDog(void)
{
dwdReset(WDOG_REG); //reset watchdog
}
After the watchdog times out and the MCU resets the application does not recover and nothing appears to happen, even after adding the bit below from reading the referenced post.
A couple of questions:
1.In the documentation after a watchdog timeout it talks about two options, a reset occurring or a Non Maskable Interrupt occurring, how is this configured for the non-windowed watchdog or is the only choice a reset?
2. In the documentation specifically the 'System Exception Status Register' it states the flag for the a watchdog reset is at bit 13, in the example in the referenced post it uses the bit which in the docs says bit 12 is not used...
From your example I have added the following the HL_sys_startup.c
case WATCHDOG_RESET:
case WATCHDOG2_RESET:
/* USER CODE BEGIN (15) */
_memInit_();
if (_errata_SSWF021_45_both_plls(PLL_RETRIES) != 0U)
{
/* Put system in a safe state */
handlePLLLockFail();
}
_coreEnableEventBusExport_();
systemInit();
_coreEnableIrqVicOffset_();
vimInit();
esmInit();
/* USER CODE END */
break;
Why is the case statement WATCHDOG_RESET not used, what is it there for in the case statement?
Thanks