Part Number: AM263P4
Tool/software:
On our board, we will only use flash for loading program data at boot time (we do not use XIP) and for writing new program images with in-app update.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM263P4
Tool/software:
Hi Andy,
Thank you for the query.
for writing new program images with in-app update.
From my understanding, In -app update needs a Read-While Write flash part(RWW). IS25LX256-JHLE is standard part. You will need to use IS25LX256-LHLE - RWW part as per ISSI datasheet.
Can you advise us if directly connecting the OSPI flash RESET# to the AM2634P WARMRSTn output is sufficient?
Yes , This is sufficient for majority of the cases as explained by you.
I will need to confirm the *worst_case* scenario from the HW engineer. I will get back on this.
Thanks & Regards,
Rijohn
Hi Andy,
Adding on to what Rijohn mentioned above, I would suggest connecting the RESET# pin of flash in a similar manner to what is done on our EVMs by passing both the WARMRSTn and OSPI0_RESET_OUT0 (from AM263Px) through an OR logic(since these resets are active low, use AND gate) to generate a reset for RESET# pin. This is needed since if there is any case where the OSPI flash needs to be reset but the AM263Px controller is not to be reset, then this OR logic would be needed. So, we would recommend using both WARMRSTn and OSPI0_RESET_OUT0 for the RESET# logic.
I think if this were to happen, the ROM bootloader would fail to read OSPI flash then attempt to load the SBL, which is fine
Can you please elaborate on the above?
Because if ROM bootloader were to fail to Read OSPI in the sector being erased, it would try to boot from the Redundant boot locations as seen in below Table 5-10 from AM263P Technical reference manual.

Thanks,
Tejas Kulakarni
Rijohn, Tejas,
Thank you for the detailed responses. I see the use case for connecting OSPI0_RESET_OUT0 by logic OR gate, and will note it going forwards.
>> I think if this were to happen, the ROM bootloader would fail to read OSPI flash then attempt to load the SBL, which is fine
> Can you please elaborate on the above?
Sure I can be clearer.
We set Boot mode pins to OSPI Read with UART fallback. I think the worst case scenario would be if the AM263 issues a command to erase a flash sector, then AM263 resets. That would trigger the flash to reset by WARMRSTn output, and the flash chip should take 1s to recover from reset. During that 1s period, I believe the flash chip will not respond to *any* commands. So In that case I expect the RBL attempt to read the SBL from all 4 fallback addresses and fail every time because the flash chip is not responding. Then I expect RBL to switch to UART fallback boot mode; from there we can recover the system.
About the LHLE part. Our app does not use XIP flash. I think we would only need the LHLE for RWW flash operations if we needed to support in-app update and XIP. Is there another use case where we would need the RWW operation?
Is there another use case where we would need the RWW operation?
No Andy, RWW is used primary for OTA application