Part Number: MSPM0G3107
Tool/software:
Just trying to confirm if my understanding on MCLK at BOOT is correct.
The TRM mentions SYSOSC is the clock source for MCLK at BOOT.
However, I don't see that represented in Figure 2-8 of the TRM.
Is MCLK sourced from a 4MHz SYSOSC on boot, or does SYSOSC go through the PLL circuitry and that output is MUXED to ensure it sources MCLK?
Also, I understand if high accuracy isn't required, no external clock is required for the MSPM0+, correct?
It can be setup to operate at 80MHz just from the internal SYSOSC?