Part Number: AM263P4
Tool/software:
The TRM section 13.2.1.4.6.15, table 13-146 states the CPSW latency.

Is this the worst case maximum or average?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM263P4
Tool/software:
The TRM section 13.2.1.4.6.15, table 13-146 states the CPSW latency.

Is this the worst case maximum or average?
Hi Chris,
Let me check internally with our design team and get back by tomorrow.
Regards,
Shaunak
Hi Chris,
Thanks for your patience. Please find the response from the design team below:
"The latency table below is for store-and-forward. It is measured from the end of an ingress packet to the start of an egress packet. The cut-thru latency (AM261x devices) is <1.5us in 1G mode and is measured from the start of an ingress packet to the start of an egress packet."
Regards,
Shaunak
It is a bit difficult to classify it as "best, worst or average" as it depends on the test environment such as number of packets, the test interface, duplexity, xMII interface etc. The table mentions the latency observed for 1 packet at 1G link